• BF524C xtal selection

    With a BF524C, is it advisable to use the same 24MHz crystal for both USB_XTAL and CODEC_MCLK?

    -Is the USB oscillator certain to be active at all times?

    -Would any buffering be necessary or is it possible to simply connect USB_XTALIN to MCLK?

    -According…

  • How FFT accelerator (FFTA) on ADSP-SC58x/ADSP-2158x is different as compared to ADSP-214xx processors / What are the major features of FFTA on ADSP-SC58x/ADSP-2158x ?

    FFT Accelerator on ADSP-SC58x/ADSP-2158x is a completely new design as compared to the FFT accelerator on ADSP-214xx processors. The major differences/features of the FFT accelerator on ADSPSC58x/ADSP-2158x are:

    • Unlike in ADSP-214xx, the…
  • Porting software  from ADSP-21489 to ADSP-21573 and ADSP-SC573 

    Customer ask some questions.

    Right now we have  plenty of software for ADSP-21489, but it’s quite hard to port it to ADSP-SC573 family. Code itself

    is 99% C and C++.

     

    Does family ADSP-SC573 have interface with external static memory like AMI for ADSP…

  • prototyping the a ADSP-TS203S design with a ADSP-TS201s or a ADSP-TS202S

    We're currently laying out a prototype PCB to take an ADSP-TS203 TigerSHARC
    Processor (i.e. with only a 32 bit cluster bus and 2 link ports). Could we fit
    an ADSP-TS201/2 to this board if we constrict external bus access to 32 bits
  • How DMC/DDR controller in ADSP-SC58x/ADSP-2158x different than DDR2 controller on ADSP-2146x ?

    ADSP-2146x

    ADSP-SC58x/ADSP-2158x

    Supports only DDR2 memory devices Supports DDR3, DDR2, and LPDDR memory devices
    Supports maximum clock/data rate of 225/450 MHz Supports maximum…
  • ADSP-SC5xx/ADSP-215xx

    EngineerZone technical forum that provides customer support for Analog Devices ADSP-SC5xx/ADSP-215xx products.
  • How IIR accelerator on ADSP-SC58x/ADSP-2158x is different than the FIR accelerator on ADSP-214xx?

    The IIR accelerator on ADSP-SC58x/ADSP-2158x works exactly in the same manner except the following differences:

    • Unlike in ADSP-214xx, you don't need to enable the IIR accelerator in PMCTL1 register explicitly in ADSP-SC58x/ADSP-2158x. In fact…
  • How FIR accelerator on ADSP-SC58x/ADSP-2158x is different than the FIR accelerator on ADSP-214xx?

    The FIR accelerator on ADSP-SC58x/ADSP-2158x works exactly in the same manner except the following differences:

    → Unlike in ADSP-214xx, you don't need to enable the FIR accelerator in PMCTL1 register explicitly in ADSP-SC58x/ADSP-2158x. In fact,…

  • Is there anything equivalent to External Port DMA (EPDMA) on ADSP-214xx processors available on ADSP-SC58x/ADSP-2158x processors?

    ADSP-SC58x/ADSP-2158x processors support two options to transfer the data between different on-chip and off-chip memories:

    1. MDMA: These are completely new as compared to the EPDMA on ADSP-214xx processors. The programming model of these…
  • ADSP-21573/ADSP-SC573 and external SRAM

    Good day! I have simple question about ADSP-21573/ADSP-SC573. Can external memory controller of ADSP-21573 and ADSP-SC573 work with external SRAM? There is some SMC - this is what we need or it's for something else? We need an analog of AMI from 489 family…