• The difference between ADSP-BF523 and ADSP-BF522 When used Host DMA

    Hi:

    I'm a disty dedicated FAE for ADI, Now there is a issues about ADSP-BF522 in my customer:

    They used ADSP-BF523 with Host DMA Download, it worked normally, and it's mass production;

    When it's replaced by ADSP-BF522 with no change in the…

  • ADSP-BF523 Power Supply Failure

    Hi,

    i have a Problem with the ADSP-BF523 that the 1V2 are causing an short circuit to the power supply.

    I am using an external 3v3, 2v5 and 1v2 power supply.

    Can you provide me an hint, what event can damage the dsp to show such a failure.

    Thanks

  • RE: BF527 Multi-cycle Instructions and Latencies. any document?

    yes,

    e.g. in the datasheet of BF-527, it sais the family has following processors:

    ADSP-BF522/ADSP-BF523/ADSP-BF524/ADSP-BF525/ADSP-BF526/ADSP-BF527

    but you said previously

    "2) The ADSP-BF531/ADSP-BF532/ADSP-BF533 processors belong to the same…
  • RE: BF523 SPI EMUEXCPT

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: Update 8 Breaks Stand-alone Flash Programmer

    Hi Alex,

    as VisualDSP++ 5.0 was released almost 3 years ago, there have been a number of bug fixes and improvements to the tools throughout the updates we have issues in that time.

    Attached is the release note from VisualDSP++ 5.0 Update 8. This Release…

  • RE: power up sequence for BF527

    Hi,

    The anomaly will appear in Rev D of the BF522/4/6 list and Rev F of the BF523/5/7 list. We anticipate that the updated BF522/4/6 list will appear online at the end of the month and the BF523/5/7 list will go online sometime next month.

    -Joe

  • RE: gstack-like utility

    Hi,


    I'm not sure how useful this is but from VisualDSP++ Update 9 we added support for detecting when an application's stack size increases beyond its allocated size. You will find more information on page 9-8 of the attached Release Note for Update…

  • TAGS LIST: Blackfin Processors

    LABVIEW_EMB_BF
    LABVIEW-SBF
    TOOLS-MISC
    ADSP-BF504
    ADSP-BF504F
    ADSP-BF506F
    ADSP-BF512
    ADSP-BF512F
    ADSP-BF514
    ADSP-BF514F
    ADSP-BF514F16
    ADSP-BF516
    ADSP-BF516F
    ADSP-BF518
    ADSP-BF518F
    ADSP-BF518F16
    ADSP-BF522
    ADSP-BF52…
  • BF527 PLL setting

    Could you explain me which way of PLL setting for BF527 is correct?

    There is information:

    "Note that the divisor ratio must be chosen to limit the system

    clock frequency to its maximum of fSCLK. The SSEL value can be

    dynamically changed without…

  • RE: BF527 power up sequence

    Hi Eamonn,

    Although Blackfin processors have no power-up sequencing requirements, a silicon anomaly on existing ADSP-BF527 silicon revisions (0.0, 0.1 and 0.2) may lead to PLL issues when VDDINT is powered before VDDEXT. This very same issue is discussed…