• BF512F - SPORT1 RX Interrupt not working - AD73360

    Hi,

    I've got a BF512F (custom board) setup with a AD73360 A/D via SPORT1. I have attached my code. I send the control words via the SPORT succesfully to the A/D. I've checked the signals on the scope and they all look fine. I can see the A/D receives…

  • Using the internal SPI flash in the BF512F

    Hi,

    I'm starting to design a prototype using the BF512F. I have a couple things in mind for the internal SPI flash. I want it to do three things:

    1) Contain the program code that will get loaded into instruction SRAM on bootup.

    2) Contain nonvolatile…

  • Place a table at an absolute address - BF512F

    Hi,

    I have finished my code for a project. I store the binary file on the internal SPI flash of the BF512F. I've got the BF512F to boot from flash etc. Everything is running 100%.

    What I want to (have to) do now to finish the project off is, I…

  • Using SPI1 and RSI interface together on the BF512F

    On the BF512F, I see that SPI1 and the RSI interface share pins. Is it possible to use them both at the same time?

    Thanks,

    Steve.

  • how to protect the code in the bf512f

    hi

    everybody,  I find that ADI have supplied the lockbox function .but I think it is very difficult to use it .do you have any good idea to protect our code ?

    because we program the fllash by JTAG.

    do  the code can  be read from the flash through the…

  • Code to Flash - BF512F - Booting from internal flash

    Hi,

    I have a custom board but can not get my code to run from the internal flash. I did a simple led_blink application to test with. I have followed the following steps http://ez.analog.com/message/27456. I am not using SDRAM yet, but have anyways made…

  • BF512F - SPI1 in DMA mode: how to enable interrupts?

    Hello all,

    I'm using BF512F and I would use SPI1 in DMA mode, but looking into the DSP's Manuals I'm not able to find how to enable Rx/Tx Interrupts in this case.

    Moreover, only "adi_int_SICEnable(ADI_INT_DMA7_SPI0)" command is recognized…

  • How many instances does UART have in ADSP-SC59x/ADSP-2159x processor?

    How many instances does UART have in ADSP-SC59x/ADSP-2159x processor?
  • How FFT accelerator (FFTA) on ADSP-SC58x/ADSP-2158x is different as compared to ADSP-214xx processors / What are the major features of FFTA on ADSP-SC58x/ADSP-2158x ?

    FFT Accelerator on ADSP-SC58x/ADSP-2158x is a completely new design as compared to the FFT accelerator on ADSP-214xx processors. The major differences/features of the FFT accelerator on ADSPSC58x/ADSP-2158x are:

    • Unlike in ADSP-214xx, the…
  • Porting software  from ADSP-21489 to ADSP-21573 and ADSP-SC573 

    Customer ask some questions.

    Right now we have  plenty of software for ADSP-21489, but it’s quite hard to port it to ADSP-SC573 family. Code itself

    is 99% C and C++.

     

    Does family ADSP-SC573 have interface with external static memory like AMI for ADSP…