• VisualDSP++ 5.0 ADSP-BF506F EZ-KIT

    To support the new ADSP-BF506F EZ-KIT, we have just released the VisualDSP++ 5.0 ADSP-BF506F EZ-KIT .  This release is based on VisualDSP++ 5.0 Update 7.  It includes support for the ADSP-BF50x processor series, including device drivers, system services…

  • FAQ: ADSP-BF506F FLASH Tutorial

     

     

     

    Q. How can I effectively debug an ADSP-BF50x project that uses both internal memory and FLASH?

     

     

     

     

     

    --------

     

     

     

     

     

    A. The ADSP-BF50x processor series is a little different to develop and debug code for as there is no access…

  • ADSP BF506F EZ kit Lite - PWM generation

    Hi,

    Presently I am working on ADSP BF506F processor, and I want to generate a single phase PWM waveform. I configured all the registers and enabled ports to connect to the oscilloscope. The code is attached and I connected to the P314 and P31 ground…

  • ADSP-BF506F EZ-KIT Lite ADC input Range

    Hi,

    Can someone tell me whether the ADSP-BF506F EZ-KIT Lite ADC configuration accept bipolar input?

    Thank you.

  • FAQ: Can’t connect to the ADSP-BF592 or ADSP-BF506F EZ-KITs after upgrading to CCES 1.1.0

    Question:
    After upgrading to CrossCore Embedded Studio 1.1.0, I can no longer connect to the ADSP-BF592 or ADSP-BF506F EZ-Kit. What’s changed?

     

    ---------------------------------

     

    Answer:

    CCES 1.1.0 introduces a new driver for the ADSP-BF592 and…

  • ADSP-BF506F EZ-KIT Lite USB Communication Interrupt

    Hi!

    I got a problem conncting my KIT to the VisualDSP by using the Debug Agent.

    The ADSP-BF506F EZ-KIT Lite is powerd by a 5VDC (890mA max) source. When I connect the USB cable to the target and to the PC, the yellow and green LED's on the target …

  • RE: Board dimensions of the ADSP-BF506F EZ-KIT Lite

    Hi David,

    The side with the DB-9 connector is 4.8". The file I'm looking at is a PDF in the layout folder of the ADSP-BF506F EZ-KIT-LITE Design Reference.

    Best Regards,

    Joe

  • Problem in Quadrature Encoder Mode Counter in ADSP-BF506F EZ-KIT Lite

    i m confuse in Quadrature Encoder Mode Counter in ADSP-BF506F EZ-KIT Lite...got any example to help...thks

  • ADSP-BF506F: How to code circular buffer?

    Hello,

    I used ADSP-2181 where I used to write a code for circular buffer as following.

    .VAR/CIRC comm[32];

    .

    .

    .

    L0=32;

    I0=comm;       

    M0=1;

    .

    .

    .

    I0=comm; // point to beginning of comm[32] vector
    CNTR=32;
    AX0=0x0000;
    DO comm_zero UNTIL CE;
    comm_zero…

  • RE: VDSP++ 5.0, ADSP-BF506F, LED 0.5 Hz Hello World Problem

    Hi,

    attached is a simple example that sets up the timer and an ISR, then uses two 'blink LED' functions - one in flash, one in internal memory - to blink the LEDs at a period defined by a timeout value #define.

    Hopefully that serves as a good…