• ADSP BF504

    Do Visual DSP++ 5.0 support ADSP BF504? Do I have to upload it to Update 8?

  • RE: ADSP BF504 spi flash


    Hi,

    Please refer the ADSP-BF504 webpage. which contains the detailed information about ADSP-BF504  and corresponding documents for this DSP.
    www.analog.com/.../adsp-bf504.html

    Note that the ADSP-BF504 provides flexible booting options from internal flash…

  • Replacement for the ADMCF340

    Hi,

    Need to do a board spin since the ADMCF340 is obsolete. 

    This is being used for motor control and required fixed point DSP.

    Is the ADSP-BF504 the closest choice?

  • Can ADSP-BF504 peripheral configuration

    Is it possible to configure the ADSP-BF504 (88 pins) to have two SPORTS (just need to receive only) and one PWM channel (3-phase)?  Looking at Table 9-1 to 9-3 in ADSP-BF50x Blackfin Processor Hardware Reference it does not seem possible to have 2 SPORTs…

  • RE: Error in the last link for ADSP-BF700 project

    OK, I just answered my own question.  The old ADSP-BF504 project I am basing this on has a LOT of spaces in the project name.  I got rid of the spaces "MAX Wireless Base Take II" -->> "MAX_Wireless_Base_Take_II" and  all of my …

  • RE: Power consumption on BF504B(no internal flash)

    Hello Loc,

    It's likely that you're seeing anomaly #05000495. You can see the anomaly details in the ADSP-BF504/BF504F/BF506F Blackfin Anomaly List here:

    http://www.analog.com/en/processors-dsp/blackfin/processors/ic-anomalies/resources/index…

  • Unstable JTAG connection to target board

    Hi

    I have the analog devices ADZS-USB-ICE and trying to connect it to the ADSP BF504 on my DSP board.  May be 1 out of 10 times I can establish a connection but most of the time I can't.  Every time it failed to establish a connection I ran ICE test…

  • external SPI flash driver for BF504

    Hello,

    I have to implement a flash driver for using an external SPI Flash memory with ADSP-BF504.

    The flash part is SST26VF032BA.

    I started with the existing driver for m25p16 that I found in the ADSP-BF506F folder.

    I can load the driver:

    I can erase…

  • BF504 memory

    Hello,

       1) I need to have two buffers, as large as it is possible, 16000B could by enough for each(more would be better..). So I tried to save one buffer in L1_CODE and second one in L1_DATA, but from picture below I can see that in L1_DATA is not enoug…

  • TAGS LIST: Blackfin Processors

    LABVIEW_EMB_BF
    LABVIEW-SBF
    TOOLS-MISC
    ADSP-BF504
    ADSP-BF504F
    ADSP-BF506F
    ADSP-BF512
    ADSP-BF512F
    ADSP-BF514
    ADSP-BF514F
    ADSP-BF514F16
    ADSP-BF516
    ADSP-BF516F
    ADSP-BF518
    ADSP-BF518F
    ADSP-BF518F16
    ADSP-BF522
    ADSP-BF52…