Good day! I have simple question about ADSP-21573/ADSP-SC573. Can external memory controller of ADSP-21573 and ADSP-SC573 work with external SRAM? There is some SMC - this is what we need or it's for something else? We need an analog of AMI from 489 family…
在BF518BF16页面下找到的硬件参考手册当中,封面上写的是Includes ADSP-BF512, ADSP-BF514,ADSP-BF516, DSP-BF518,没有包含518F16 ,也没有勘误表
请问BF518的硬件参考手册和BF518F16有区别吗?
硬件参考手册能使用同一个吗?
Attached memory test can be used to test DDR memory (or any other memory type or memory mapped peripheral) on ADSP-2156x processor. The test is performed for different types of accesses (e.g., core, DMA, 8-/16-/32-/64-bit) and different data patterns…
Hi,
Please see the attached example code which allows the link port to be tested on the ADSP-SC589 EZ-KIT. The setup requires the ADSP-SC589 EZ-KIT and the EI3 Probing adapter.
The attached code configures the link ports in DMA stop mode and transfers…
ADI announced today its next generation floating-point SHARC processor, the first dual-core floating-point processor in the portfolio, featuring two improved SHARC+ cores (ADSP-2158x series) and an optional ARM Cortex-A5 core (ADSP-SC58x series). For…
Hello,
ADSP-SC587 interfaced with ADSP-BF561 through SPORT in our custom board, issue is when we set clock frequency 1 MHz communication between the processor is fine. But when we increase the clock frequency, clock is getting deteriorated. Our requirement…
Sir,
Do you have ADSP-21479 & ADSP-21584 OrCAD symbol?
If not, could you help export EZ-kit's file then it can be imported to OrCAD.
My customer uses OrCAD and need the symbol library.
Thank you,
Kris
Hi Mussab,
The code I used was the same which comes along with the ADSP-SC5XX Board Support Package available at the link below:
ADZS-SC589-EZLITE Evaluation Board | Analog Devices
at the path:
"..\ADSP-SC5xx_EZ-KIT\Examples\drivers\fft\SmallFFTDescriptorChain…
http://download.analog.com/tools/CrossCoreEmbeddedStudio/Releases/Release_2.8.0/CrossCoreEmbeddedStudio_2.8.0_Release_No…
5.3 ADSP-SC57x/ADSP-2157x Processors Running at 500 MHz
The manual says, the ADSP-SC57x/ADSP-2157x processor is configured for…