• [Ask] ADSP-21587 529-BGA Ball Assignment

    Sir,

    My customer are drawing ADSP-21587 schematic and layout.

    There is one question in 529-BGA ball assignment.

    Datasheet only describe full function ball assignment like ADSP-SC589.

    ADSP-21587 has same package, 529-BGA, but less functions.

    No…

  • ADSP-21587 SHARC+ Static Memory Controller setup

    Hello,

    I'm trying to use the Static Memory Controller (SMC) of a ADSP-21587 to connect an LCD module.  The module has a normal parallel interface 16 bits wide, a register select pin for writing command or data, a ~RE, ~WE, and a ~CS.  I've used the…

  • unused pin for 21587

    Hi Sir,

    We are designing the ADSP-21587 and reference SC589 since they share the same datasheet and EVB. Compare w/ SC589, the ADSP-21587 doesn't support SD/SDIO/eMMC (MSI), MLB, EMAC, USB, and PCIe function (table 2 of datasheet).

    As study the table…

  • RE: Bounary Scan with ADSP-SC58x and ADSP-21584

    Hi EZAdmin,

    Can I get the updated datasheet? I would like to know if this issue has been resolved in any other revision of the device/die(ADSP-SC587BBCZ-5).

    -- BSDL File
    -- File Name: ADSP-2158x_ADSP-SC58x_529CSPBGA.bsdl
    -- File Revision: 0.0
    -- Date Created…

  • How FFT accelerator (FFTA) on ADSP-SC58x/ADSP-2158x is different as compared to ADSP-214xx processors / What are the major features of FFTA on ADSP-SC58x/ADSP-2158x ?

    FFT Accelerator on ADSP-SC58x/ADSP-2158x is a completely new design as compared to the FFT accelerator on ADSP-214xx processors. The major differences/features of the FFT accelerator on ADSPSC58x/ADSP-2158x are:

    • Unlike in ADSP-214xx, the…
  • Porting software  from ADSP-21489 to ADSP-21573 and ADSP-SC573 

    Customer ask some questions.

    Right now we have  plenty of software for ADSP-21489, but it’s quite hard to port it to ADSP-SC573 family. Code itself

    is 99% C and C++.

     

    Does family ADSP-SC573 have interface with external static memory like AMI for ADSP…

  • prototyping the a ADSP-TS203S design with a ADSP-TS201s or a ADSP-TS202S

    We're currently laying out a prototype PCB to take an ADSP-TS203 TigerSHARC
    Processor (i.e. with only a 32 bit cluster bus and 2 link ports). Could we fit
    an ADSP-TS201/2 to this board if we constrict external bus access to 32 bits
  • How DMC/DDR controller in ADSP-SC58x/ADSP-2158x different than DDR2 controller on ADSP-2146x ?

    ADSP-2146x

    ADSP-SC58x/ADSP-2158x

    Supports only DDR2 memory devices Supports DDR3, DDR2, and LPDDR memory devices
    Supports maximum clock/data rate of 225/450 MHz Supports maximum…
  • ADSP-SC5xx/ADSP-215xx

    EngineerZone technical forum that provides customer support for Analog Devices ADSP-SC5xx/ADSP-215xx products.
  • How FIR accelerator on ADSP-SC58x/ADSP-2158x is different than the FIR accelerator on ADSP-214xx?

    The FIR accelerator on ADSP-SC58x/ADSP-2158x works exactly in the same manner except the following differences:

    → Unlike in ADSP-214xx, you don't need to enable the FIR accelerator in PMCTL1 register explicitly in ADSP-SC58x/ADSP-2158x. In fact,…