• ADSP-21571 Interface to FPGA

    Hello, I'm still using the TigerSharc ADSP-201 DSP and interface to an FPGA over the external Data/Address bus. The interfacing to FPGA was very easy and very powerful using the Pipeline protocol. I was looking at the latest Sharc processor and foudn…

  • Implementing GIGE UDP on ADSP-21571?

    Hello, I was wondering if there are any example code for the ADSP-21571 that implements GIGE using UDP packets?

    Do you need an real-time operating system?

    Thanks,

    Joe

  • ADSP-21571 SPI Slave Boot problem

    Hi,

    I'm trying to boot an ADSP-21571 using SPI Slave mode, but I just can't get it to work.
    I'm pretty sure I have configured my SPI Master correctly (msb-first, pos. clk polarity). At the moment I'm running at a very low rate (1MHz).

  • About JTG-TRST processing of ADSP-21571

    Hello.

    Please tell me about JTG-TRST processing of ADSP-21571.

    About R72 / R73 of JTG-TRST line of ADSP-SC573 EZ-KIT schematic diagram,

    The schematic diagram and board of the ADSP-SC573 EZ-KIT are in the following state,

    Please tell me which of the…

  • About the C2_FLG2 signal of ADSP-21571

    Hello

    I would like to use the C2_FLG2 signal of ADSP-21571 (LQFP176), but if I check the data sheet

    In Table 20, PC_15

    In Table 23, PC_10

    Which one is correct?

    Best regards.

  • Maximum external TMR_CLK frequency for ADSP-21571

    I am reading the ADSP-SC570/SC571/SC572/SC573/ADSP-21571/21573 datasheet, rev.B.

    I would like to know the maximum  external TMR_CLK frequency.

    On page 102, the datasheet states: "for the external TMR_CLK maximum frequency, see the fTMRCLKEXT specification…

  • About GriffinLite ADSP-21571 support for MOST without ARM core

    I am considering the product specification of GriffinLite ADSP-21571.

    Can GriffinLite ADSP-21571 without ARM core support MOST?

    Please let me know if you have usage instructions and reference documents.

  • ADSP-21571: Linkport DMA bandwidth control or similar

    Hi all,

    I'm receiving 32-bit data over the Linkport. The Linkport FIFO is emptied by the Linkport DMA (DMA36 for ADSP-21571).

    Now, I need to briefly stop the DMA/Linkport. Is there an easy to do this? Using the DMA (or Linkport) enable bits (in corresponding…

  • ADSP-21571/ICE-2000: Not able to connect to target

    Hi,

    I'm trying to debug a custom board with two ADSP-21571 and one ADSP-21489.

    As I am focusing on debugging the 21571s I've marked the 21489 as "Unknown" in the Target Configurator (I'm new to CCES, but I get the feeling you cannot debug different…

  • (ADSP-21571)About SPI(non-DMA) TFIFO

    Hi

    I use SPI0 (slave) with non-DMA.

    The settings are as follows.

    - SPI0_CTL.SIZE = 2(32bit word)

    - SPI0_CTL.SIZE = 1(Enable)

    - SPI0_TXCTL.TDU = 1(Send zeros when SPI_TFIFO is empty)

    I want to output data in synchronization with the clock from the…