Question
The Startup Code/LDF settings in the System Configuration provide three options to partition SDRAM: "Custom", "Default", or "None". When selecting 'None' for the BF561/BF609 why do I receive this error?:
…Question
The Startup Code/LDF settings in the System Configuration provide three options to partition SDRAM: "Custom", "Default", or "None". When selecting 'None' for the BF561/BF609 why do I receive this error?:
…Here is an example code for Core timer with Interrupts on a SHARC+ Core in ADSP-SC58x/ADSP-215xx.
There are two CRC blocks CRC0/CRC1 present in ADSP-SC58x/ADSP-2158x processors. CRC0 is tied with MDMA0(8→9) stream and CRC1 is tied with MDMA1 (18→19) stream.
A software library containing support for using the FFTA is provided with the CrossCore Embedded Studio. Using this library, C or C++ programs running on an ARM Cortex A5 or SHARC ADSP-215xx and ADSP-SC5xx core can access the FFTA to implement various…
There are maximum of 2 DMC controllers present on ADSP-SC58x/ADSP-2158x processors. For more details, refer to the processor data sheet.
FIRA Performance
The FIRA processing mainly consists of the following stages:
FIRA runs at SCLK0 on ADSP-SC58x/2158x and ADSP-SC57x/2157x processors. FIR compute…
Yes, like other peripheral DMA channels, MDMA also support descriptor based modes (descriptor array, descriptor list, descriptor on-demand etc.).
Q:
The ADSP-21371 in commercial temperature grade has two part numbers, one with suffix -2A and another with suffix -2B. What are the differences between the two parts?
---------
A:
On the ADSP-21371 there are no audio algorithms in ROM, just the coefficients…