Hi Anand,
Thanks for your reply, the asynchronous sample rate converter example is not available in the ADSP-21479 board support package.
I downloaded the example as part of the ASCR SHARC software module:
Hi Anand,
Thanks for your reply, the asynchronous sample rate converter example is not available in the ADSP-21479 board support package.
I downloaded the example as part of the ASCR SHARC software module:
Hello,
I have the ADSP-21479 EZ-BOARD and I am having issues with downloading SigmaStudio project
I am booting from parallel flash (SW4 set to position 2). but I also trying loading the LDR via SPI slave boot with same result.
I get the following LED…
Hi,
You can get the bare metal framework from the ADSP-21479 (Board support package). Please click on the below link to download BSP for ADSP-21479.
download.analog.com/.../ADI_ADSP-21479_EZKIT-Rel1.0.0.exe
After installing the BSP, you would get the example…
系统框架是:ADSP-21479 + ADAU1466 + MIC_ADC + AMP
关于clock同步实现方式如下:
1、ADAU1466作Master,生成BCLK、FSYNC。
2、21479配置DAI SRU直接将1466过来的BCLK、FSYNC引脚信号内部分别路由到 ADC和AMP芯片对应的BCLK、FSYNC引脚上。
调试发现以下问题:
有时候系统上电,21479虽然能采集到1466和ADC的数据,能产生SPORT接收DMA中断,但经分析数据是异常的(像是采集不同步)。
这时,假如将系统重上电…
Hello,
I am using the ADSP-21479 EZ-Kit and tinkering with the example code for SPDIF to Analog talk through with SRC.
I am trying to program a "No Stream Error" to occur whenever the audio stream is disconnected from the S/PDIF receiver.
How…
Hi Lee,
Apologies for the delay.
Please find the attached SPI slave booting code for ADSP-21479 processor. This code can be tested across two ADSP-21479 EZ-Kits, where one can be configured as host processor that sends the loader file and other can be act…
How do you solve this problem? can you share your code to me? I am meeting the same problem too now. very thanks.
Hi,
Apologies for the delayed response.
Were you able to get going. Let us know if you are still facing any issues.
Can you please get back to us on the below points? it will help us to assist you better on this.
1) Can you please explain how you are generating…
I am trying to simulate an app on the ADSP-21479.
I don't need any real-time I/O so simulation is fine.
I have tried both CCES_runner and chipfactory.
Here are the outputs :
CCES_runner.exe --target "ChipFactory Simulator" --processor ADSP-21479 -…
Dear support,
I have assembled the simple circuit in the SigmaStudio for SHARC, where I've used the Square wave module with a frequency of 50 Hz:
I've sent a signal to the S/PDIF or analog pins and see the slopes:
As I understand, the board does not…