• RE: ADSP INTERNAL RAM TEST

    the manual said " To modify these files, you need proficiency in ADSP-21xxx assembly language......",   where can i get the  "ADSP-21xxx assembly language" manual .  I think this  manula will help me .

    thanks a lot.

  • CLDP DRIVER FOR ADSP-21584

    To write SPI flash memory with CLDP.EXE, I need to install drivers for each device.

    I am looking for a driver for ADSP-21584.
    Please let me know where to find it.
    If you can divert it for other devices, that is still fine.
    Perhaps it does not exist and I…

  • ADSP-21562

    Hi

     Would you pls help to check below question., thanks 

    1)Does it need special configuration for  SPORT1 ?  or there is referance code ? it' can't work when refer SPORT0、2、3 configuration that SPORT0、2、3 can work .

    2) Can DAI0 data be routed to DAI1 output…

  • ADSP-21562

    Hi

     Would you pls help to check below question., thanks 

    1)Does it need special configuration for  SPORT1 ?  or there is referance code ? it' can't work when refer SPORT0、2、3 configuration that SPORT0、2、3 can work .

    2) Can DAI0 data be routed to DAI1 output…

  • Minimum SCLK in ADSP-21562

    Hi

    What is the minimum SCLK for the ADSP-21562, I can work with?

    Can I program fCCLK to 200 or 100 MHz in ADSP-2156x processors

    best George

  • FAQ: ADSP-21569 SPI Host example

    Attached is the ADSP-21569 SPI Host example and the connection diagram to boot the another DSP via SPI slave boot mode. This code is verified between two ADSP-21569 Ez-kits.

    Normally, all the slave booting process is done as, the Host Application would…

  • ADSP-2156x 120-Lead LQFP reference schematic

    There doesn't seem to be any hardware reference design for the ADSP-2156x SHARCS with the 120-Lead LQFP package.

    Specifically, for power supply bypassing.

    In the schematics for the 21569 EZ-Kit etc. the bypassing scheme is best described as.... random…

  • ADSP-21565 max CLKIN0 frequency

    Hello

    The data sheet for the ADSP-21565 specifies that the max CLKIN0 freq is 30MHz, however I would like to ask whether there would be any issues if I was to drive it with at 40MHz (as I have done previous (legitimately) with SHARC DSP processors such…

  • ADSP-21569 API Documentation

    Hello,
    I would like to use the provided hardware drivers for the ADSP21569. For example: In the provided examples the functions defined in "adi_sport_2156x.h" are usedto set up serial comunication such as TDM. I would like to do so aswell.
    Sadly…

  • RE: Verify ADSP -21584 / SC584 Clock rate

    Hi,

    As per the datasheet, ADSP-21584BBCZ-4A supports maximum Processor Instruction Rate of 450MHz at –40°C to +85°C . We cannot guarantee the proper operation of the devices if the specification not followed. So, we would suggest you to follow the specifications…