• RE: Speaker Equalization with the ADSP-21366 + ADSP-21367

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADSP-21367/369 differencies

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • the difference between ADSP-21363KBCZ-1AA and ADSP-21369

    Hello ADI Colleagues,

    One of our customers would like to update their hardware with ADSP-21369 to replace ADSP-21363KBCZ-1AA. Do they need to modify their hardware and software?

     

    Thanks & Best regards,

    xiangzhi wu

  • FAQ: How does target initialization differ in ADSP-SC598 vs ADSP-SC57x/8x?

    Target initialization, including system reset, is performed as part of the Cortex-A55 OpenOCD target initialization for ADSP-SC598. If only the SHARC cores are being debugged in ADSP-SC598, a core reset is performed on each loaded core and no system reset…

  • What are the key differences between the ADSP-SC598 and ADSP-SC594 processors?

    What are the key differences between the ADSP-SC598 and ADSP-SC594 processors?

  • Announcing Yocto Linux for ADSP-SC5xx 2.0 (Beta for ADSP-SC589 EZ-Kit only)

    Hi all,

    I'm pleased to announce that we have released a public beta of the 2.0 release of Yocto Linux for ADSP-SC5xx.

    The beta release currently contains support for the following development boards:

    • ADSP-SC589 EZ-Kit

    Other boards will be added…

  • What are the differences between EMAC on ADSP-SC598 processor family as compared to ADSP-SC594 processor family?

    What are the differences between EMAC on ADSP-SC598 processor family as compared to ADSP-SC594 processor family?

  • ADSP-21367-DMA FIFO Status

    Hi I am using External port DMA for reading an arrray of data from SDRAM in ADSP-21367 processor.

    I am not using External port DMA interrupt to check the DMA completion.

    I am checking  only the EXTS bit

    #define EXTS        (BIT_24)

    Wait_for_DMA_Complete: 

  • [ADSP-SC594] PDM function

    Hi,

    I am using ADSP-SC594. I want to receive audio data from 4 digital microphones using the PDM interface. I tried the following, but the desired SDATA output is not coming out.

    Hardware connections are Clock - DAI1_05, Data0 - DAI1_07, Data1 - DAI1_08…

  • FrameSyncError (ADSP-21569)

    Dear sir,

    Hello.

    Could you tell me the mechanism and cause of Frame Sync Error of SPORTs?

    And, What will happen, when Frame Sync Error is occurred?