• RE: Speaker Equalization with the ADSP-21366 + ADSP-21367

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADSP-21367/369 differencies

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADSP-21367-DMA FIFO Status

    Hi I am using External port DMA for reading an arrray of data from SDRAM in ADSP-21367 processor.

    I am not using External port DMA interrupt to check the DMA completion.

    I am checking  only the EXTS bit

    #define EXTS        (BIT_24)

    Wait_for_DMA_Complete: 

  • ADSP-21363BSQZ

    What is difference between

    ADSP-21363BSQZ and

    ADSP-21363BSWZ ?

  • Questions on ADSP-21489

    Hi

    I am trying to port some speech processing algorithms on  ADSP-21489, have below questions. Using ADSP-21489 EZ-Board for testing purpose.

    1. Does  ADSP-21489 has data cache? when I tried to read/write from external memory, it takes 30 odd cycles whereas the…
  • How many instances does UART have in ADSP-SC59x/ADSP-2159x processor?

    How many instances does UART have in ADSP-SC59x/ADSP-2159x processor?
  • blackfin ADSP-609

    Hi,

    How can we kickstart core 0 to core 1 in blackfin ADSP-609....

  • ADSP-21489 display

    I would like to know if a dsp chip like the ADSP-21489 can be connected directly to a touch screen display, encoders and buttons or it is necessary a second microprocessor for these functions ?

  • Rewiew an ADSP-21565KSWZ10 site

    Hello ADI community, dear engineers I would like requre your help and professional expiriance.

    I'm junior to shematic also with SHARK processors, and unfotunnaly my job consist in the project creation of application with ADSP-21565KSWZ10 processor on…

  • FAQ: ADSP-BF592 SPI loopback

    Attached is the ADSP-BF592 SPI example code for ADSP-BF592. The connection details are mentioned in the "SPI_TX_RX_Loop.c" file.

    BF592_SPI_Loopback.zip