• ADSP-BF514 recommended SPI Flash

    Hello,

    Could you please provide a list of recommended external SP Flash ICs for ADSP-BF514KSWZ-4?

    Thanks,

    Evgeny

  • ADIN2299 - About adsp cm409f equivalent solution

    Hello to everyone

    We want to create our ethernet solution to use in our R&D Product, by referring to the "Rapid Platform Generation 2(RPG2)" available in the ADI Chronous Developer Portal.
    However,
    Due to the global chip crisis, we are having…

  • RE: ADSP-BF548BBCZ-5AA AA = low Alpha Package

    Hi,

    Apologies for delay in response.

    Technically identical product, but AA uses a superior mold compound.

    Regards,
    Anand Selvaraj.

  • RE: Connection of ADSP-SC57x to USB-C?

    Hi,

    In Type-C CCx pin is used to determine the mode of operation. Have a look on the below details,
     
    Device Mode – UFP (Upstream Facing Port) – CC1 & CC2 terminated with pull down resistor (Rd)
    Host Mode – DFP (Downstream Facing Port) – CC1…

  • Inquiries about EMC Guidelines for ADSP-SC589

    Dear ADI,

    I'd like to ask if there is a document on the EMC guidelines for ADSP-SC589.

    If there is such a document, please send it or link that website.

     

    Thank you.

     

    Best Regards,

    Inho Jeon

  • RE: ADSP-SC589_EZ-Board Analog input noise

    I could not do all tests, since I lack the necessary cables.

    Standard loop test passed.

    LED test "passed", but.no LED10/11/12 activity.

    UART test passed

    HADC test passed.

    CAN not performed, no cable.

    SPDIF coax test passed.

    SD card test passed…

  • RE: Bounary Scan with ADSP-SC58x and ADSP-21584

    Hi EZAdmin,

    Can I get the updated datasheet? I would like to know if this issue has been resolved in any other revision of the device/die(ADSP-SC587BBCZ-5).

    -- BSDL File
    -- File Name: ADSP-2158x_ADSP-SC58x_529CSPBGA.bsdl
    -- File Revision: 0.0
    -- Date Created…

  • SHARC ADSP-2156x FFT and IFFT problem

    Hi

        I have a problem about FFT and IFFT,

    I have get audio data from I2S buffer(as below real_inputBuffer_L) to push rfft:

    float real_inputBuffer_L[BUFF_SIZE/2];

    float rfft_real_output_L[BUFF_SIZE/2];
    float rfft_imag_output_L[BUFF_SIZE/2];

    float irfft_real_output_L…

  • U-boot support for USB1 in the ADSP-SC589

    We are working on a custom board design that uses the ADSP-SC589 chip and we would like to make use of the USB1 port as a TTY serial device for U-boot and Linux to use. The USB0 port is already being used to support a hub device. We are using the Yocto…

  • RE: Large FFT (32K and 64K) benchmark on ADSP-2159x