Hi,
We understand that you are using ADSP-21262. If so, currently there isn't any support for SSL/DD on earlier SHARC parts in CCES.
Also more information about importing VisualDSP++ project files into CrossCore Embedded Studio is available at:
Hello ADI Colleagues,
One of our customers would like to update their hardware with ADSP-21369 to replace ADSP-21363KBCZ-1AA. Do they need to modify their hardware and software?
Thanks & Best regards,
xiangzhi wu
Target initialization, including system reset, is performed as part of the Cortex-A55 OpenOCD target initialization for ADSP-SC598. If only the SHARC cores are being debugged in ADSP-SC598, a core reset is performed on each loaded core and no system reset…
What are the key differences between the ADSP-SC598 and ADSP-SC594 processors?
Hi all,
I'm pleased to announce that we have released a public beta of the 2.0 release of Yocto Linux for ADSP-SC5xx.
The beta release currently contains support for the following development boards:
Other boards will be added…
What are the differences between EMAC on ADSP-SC598 processor family as compared to ADSP-SC594 processor family?
Hi,
I am using ADSP-SC594. I want to receive audio data from 4 digital microphones using the PDM interface. I tried the following, but the desired SDATA output is not coming out.
Hardware connections are Clock - DAI1_05, Data0 - DAI1_07, Data1 - DAI1_08…