• Satellite Communication Using ADRV9364/61

    I was looking into satellite communication aspects using ADRV9364/61, I know it isn't designed for space applications It seems that there is some limited support in terms of bands. I want to access QO-100 satellite or may be some other satellite if you…

  • Viewing Boot Messages on the USB UART on the ADRV9364+ADRV1CCR-BOB

    After finding the windows driver for the CP2103 chip on the USB UART port P14 on the ADRV1CCR-BOB, I can run it through a boot cycle and watch what should be characters stream out over the COM port.  However, the characters are unintelligible jibberish…

  • ADRV9364-Z7020 marking

    Hi. I have a question about ADRV9364-Z7020 marking. Serial numbers and Lot number are different on the board (S19-1585 SN: 00130) and on the label (S20-0730 SN: 2020080300802). Is this acceptable? or is it a delivery error?

  • ADRV9364-z7020 evaluation board custom device tree

    Dear all,

    I have an ADRV9364-z7020 evaluation board and I'm trying to build without success a Linux image by using a customized device-tree through Petalinux v2021.1.

    After following the steps described in this Link about how to add a custom devicetree…

  • ADRV9364-Z7020

    Hi,

    Could you provide the MTBF information for ADRV9364-Z7020 & ADRV1CRR-BOB that is required for reliability analysis. 

    Olim 

  • ADRV9364-Z7020 SOM

    Hello dear support team 

    From my customer:

    We are using the ADRV9364-Z7020ADRV9364-Z7020 SOM component for a GPS application,

    during development we encounter a strange phenomenon in RF modulation:

    When modulating RF with a constant value, and expecting…

  • Implementation using ADRV9364-Z7020+FMC

    Since, FMC doesn't support HDMI when using ADRV9364 SoM, I won't be  getting a IIO scopes display where I can configure the transceiver. Is there any guide as to how to configure the hardware acting as Tx/Rx or both in a loopback mode as in ADALM…

  • ADRV9364-zc7020 operation without carrier board

    Can i use this board without connecting any carrier board, if yes then how can i achieve the same. i read in one of the thread that without carrier board it will not function. But then what is the use of the on board SD card for boot up. I was expecting…

  • Customize adrv9364-z7020

    Hello,
    
    I am new to all this and there are basic things that I do not understand in the guides provided by analog device.
    
    I want to customize my adrv9364-z7020 board. For this I saw that I must modify the device-tree 
    that comes in the linux image that…
  • static IP config whit ADRV9364-Z7020

    Hello
    Hello good day

    I have a question about the static IP config in ADRV6394-Z7020. For access to the Linux image to my board,
    Should I go into root mode? In this case, How do I do it?

    I know that the password is analog but How acces to this mode…