• Reference design for adrv9364-z720 + adrv1crr-bob and adrv9364-z720 + adrv1crr-fmc

    Hello,
    
    Currently I have the ADRV9364-Z7020 + ADRV1CRR-BOB boards, as I don't have the possibility to add an external oscillator,
    they told me that I should buy the FMC board for the ADRV9364-Z7020. As my idea is to customize the HDL reference, I…
  • Does the adrv9364 HDL reference design core implement JESD protocol?

    Hello everyone,

    I am working with ADRV9364-Z7020 and Vivado 2019.2. I would like to know if the axi_ad9361 reference design IP implements JESD protocol.

    I would like to know the configurability of clocks for util_upack2, util_rfifo and axi_ad9361 IPs…

  • DDR memory block in Simulink hdl coder, for ADRV9364-Z7020

    we are willing to implement a delay line using the ADRV9364-Z7020 board.

    In other words, take the RX port, connect to a large FIFO, and the output will go to TX port.

    This works with small FIFO, in a design we implemented with Simulink/hdl coder flow…

  • Regarding usability of ethernet ports with ADRV9364-Z7020 + FMC carrier board

    I was trying to ping from my PC to ADRV9364-Z7020 + FMC carrier board setup. While it worked with one ethernet port. The other ethernet port on FMC didn't work. Also there was no inet address when type ifconfig when connected to other ethernet port. Is…

  • ADRV9364 initialization under custom device tree with Petalinux v2021.1

    Dear Sirs/Madams,

    I am working in a project developing a custom device tree for the ADRV9364z7020 through Petalinux v2021.1.

    In a first instance, I have managed to customize in Vivado v2021.1 the original hdl with the desired interfaces. After building…

  • Building U-Boot for the ADRV9364-Z7020

    I'm trying to build U-Boot for the ADRV9364-Z7020 evaluation kit from the latest u-boot-xlnx (xilinx-v2021.2) sources because I need some configuration modification and also the Kuiper image BOOT.BIN file doesn't have a U-Boot build that supports the…

  • Linux Kernel defconfig for ADRV9364-Z7020 + ADVR1CC-BoB

    Hardware: ADRV9364-Z7020 + ADVR1CC-BoB

    Question: From this link in the 'Configure the Kernel' section it is required to follow this step;

    dave@hal9000:~/github-linux-build/linux$ make zynq_xcomm_adv7511_defconfig

    My question is - does the above…
  • ADRV9364-Z7020 support/clarification needed - bad documentation and links

    We have bought a ADRV9364-Z7020 + the PicoZed BoB

    I have spent close to two hours trying to ascertain just few basic things. I'm no longer sure if I still have the correct info and so am posting here to clarify.

    1)  My very simple question is are…

  • Ethernet Transceiver U10 on ADRV9364-Z7020 SOM - Is this Industrial or Commercial spec part?

    I'm trying to find out if the Ethernet Transceiver chip (U10) on the ADRV9364-Z7020 SOM is an industrial or commercial spec' part. The part number provided in the BOM provided by Analog Devices (link below) is incomplete.
     
    BOM:  https://wiki.analog…

  • RE: ADRV9364 appconfig.h

    Hello,

    There might be a bug with the IRQ part of the project. I haven't been able to look at it yet, but I am planning to do so in the near future.

    Regards,
    Andrei