• ADRV9364 custom board AD9364 initialization error

    We have a custom board similar to ADRV9364 + BOB. We only made the following changes on the custom board:

    1. We removed the ethernet PHY

    2. We removed the ADG77 IC as shown below, and connect the CLK output of the 40MHz crystal directly to AD9364.

  • RE: How to Move Serial Console TTY from UART1 to UART0 on ADRV9364-Z7020 and ADRV9364-Z7020?

    Hi all,

    I was able to figure it out.  I used https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/1452114088/Zynq+Linux+Pin+Controller+Driver#Devicetree as a guide.  

    Note that the following from my original post was an accident and not needed:

    &usb0 {…

  • ADRV9364-Z7020 IQ mismatch

    Hi,

    we wrote a python script using PyADI library, using the original FPGA design supplied by ADI, in which we transmit CW from the TX using DDS, and recive it in RX via leakage. than we cpature samples from the RX and take it for analysis in Matlab.

  • RE: adrv9364-z7020 noise figure problems

    AD936X device Rx ports have different impedance across the frequency band, and around 2.4 GHz impedance is ~50 ohm and that is why you are able to achieve better noise figure and impedance is ~ 200 ohms at 160 MHz, so need to do impedance matching…
  • RXA Input Power Levels-ADRV9364

    HI,

    We are planning to use ADRV9364-Z7020 for L-BAND frequencies.(950-2200)Mhz.

    what is the acceptable RF input level of the SOM.

    Required RF INPUT Level : -20dbm to -120dbm.

    Can you please recommend the attenuator which can be used with ADRV9364.

    Your…

  • ADRV9364-Z7020 new Vivado project

    Hi,

    I have recently acquired a ADRV9364-Z7020 board with the ADRV1CRR-BOB Breakout Carrier.

    To getting started, I would like to create a new project on Vivado (I use the 2018.3 version). Hovewer, when creating the project throught the Vivado wizard, I…

  • Using Openwifi on ADRV9364-Z7020 and FMC

    I was trying to boot openwifi on my ADRV9364-Z7020 with FMC carrier board. When i try using bootfiles provided on open-wifi page. After few tries it just goes into zynq boot mode . I have attched a copy of response below. Iwant to be able to run ssh commands…

  • adrv9364 write to qspi

    Hello, Is it possible to manually write to QSPI onboard mem from FPGA PL or from ARM linux when is not used to boot? what is the simplest way? the schematic shows that is connected.

    Thanks 

  • ADRV9364-Z7020+BOB reference design in VHDL

    Hi,

    I built the HDL project for my ADRV9364-Z7020 device and ADRV1CRR-BOB carrier following this tutorial (https://wiki.analog.com/resources/fpga/docs/build).

    When I open it with Vivado, all files are in Verilog. Is there a way to generate the project…

  • Reference design for adrv9364-z720 + adrv1crr-bob and adrv9364-z720 + adrv1crr-fmc

    Hello,
    
    Currently I have the ADRV9364-Z7020 + ADRV1CRR-BOB boards, as I don't have the possibility to add an external oscillator,
    they told me that I should buy the FMC board for the ADRV9364-Z7020. As my idea is to customize the HDL reference, I…