• RE: How to Move Serial Console TTY from UART1 to UART0 on ADRV9364-Z7020 and ADRV9364-Z7020?

    Hi all,

    I was able to figure it out.  I used https://xilinx-wiki.atlassian.net/wiki/spaces/A/pages/1452114088/Zynq+Linux+Pin+Controller+Driver#Devicetree as a guide.  

    Note that the following from my original post was an accident and not needed:

    &usb0 {…

  • adrv9364-z7020 noise figure problems

    Hello,

    I'm using adrv9364-z7020 + ADRV1CRR-BOB EVB and performed some noise measurements

    by sending 1 MHz CW at very low power, -80 dBm and changing the LO.

    The first thing that I noticed is that at high frequency for LO, 2.4GHz, the noise level is…

  • ADRV9364-Z7020 new Vivado project

    Hi,

    I have recently acquired a ADRV9364-Z7020 board with the ADRV1CRR-BOB Breakout Carrier.

    To getting started, I would like to create a new project on Vivado (I use the 2018.3 version). Hovewer, when creating the project throught the Vivado wizard, I…

  • adrv9364 write to qspi

    Hello, Is it possible to manually write to QSPI onboard mem from FPGA PL or from ARM linux when is not used to boot? what is the simplest way? the schematic shows that is connected.

    Thanks 

  • ADRV9364-Z7020+BOB reference design in VHDL

    Hi,

    I built the HDL project for my ADRV9364-Z7020 device and ADRV1CRR-BOB carrier following this tutorial (https://wiki.analog.com/resources/fpga/docs/build).

    When I open it with Vivado, all files are in Verilog. Is there a way to generate the project…

  • Reference design for adrv9364-z720 + adrv1crr-bob and adrv9364-z720 + adrv1crr-fmc

    Hello,
    
    Currently I have the ADRV9364-Z7020 + ADRV1CRR-BOB boards, as I don't have the possibility to add an external oscillator,
    they told me that I should buy the FMC board for the ADRV9364-Z7020. As my idea is to customize the HDL reference, I…
  • ADRV9364 initialization under custom device tree with Petalinux v2021.1

    Dear Sirs/Madams,

    I am working in a project developing a custom device tree for the ADRV9364z7020 through Petalinux v2021.1.

    In a first instance, I have managed to customize in Vivado v2021.1 the original hdl with the desired interfaces. After building…

  • Building U-Boot for the ADRV9364-Z7020

    I'm trying to build U-Boot for the ADRV9364-Z7020 evaluation kit from the latest u-boot-xlnx (xilinx-v2021.2) sources because I need some configuration modification and also the Kuiper image BOOT.BIN file doesn't have a U-Boot build that supports the…

  • Linux Kernel defconfig for ADRV9364-Z7020 + ADVR1CC-BoB

    Hardware: ADRV9364-Z7020 + ADVR1CC-BoB

    Question: From this link in the 'Configure the Kernel' section it is required to follow this step;

    dave@hal9000:~/github-linux-build/linux$ make zynq_xcomm_adv7511_defconfig

    My question is - does the above…
  • Ethernet Transceiver U10 on ADRV9364-Z7020 SOM - Is this Industrial or Commercial spec part?

    I'm trying to find out if the Ethernet Transceiver chip (U10) on the ADRV9364-Z7020 SOM is an industrial or commercial spec' part. The part number provided in the BOM provided by Analog Devices (link below) is incomplete.
     
    BOM:  https://wiki.analog…