Hi ,
Can You please provide .DSN Files for ADRV9361-Z7035
ADRV1CRR-FMC RF Som Evaluation Board
The website has PDF version of it but we require the .DSN file for our refference
Thank You
Hi ,
Can You please provide .DSN Files for ADRV9361-Z7035
ADRV1CRR-FMC RF Som Evaluation Board
The website has PDF version of it but we require the .DSN file for our refference
Thank You
Hi ADI Apps,
my customer is using the ADRV9361-Z7035 SOM in an application that is for critical infrastructure & wants to be sure that he is cooling the device appropriately.
The AD9361 datasheet claims a maximum junction temperature of 110C, and…
Someone asked by email:
-----
Where are the Ethernet MAC addresses stored in the ADRV9361-Z7035?
------
There are no plans to support E320. NI should have a reference design for the device.
-Travis
Are you using ADI eval board or custom board?
As mentioned above, if you are using crystal oscillator for the REF_clk source, then you can use the internal DCXO tuning to compensate for this drift.
Hello
hope you are doing well.
i am using ADRV9361 and didn't recvd any value.
I m running HDL Reference design branch 2019_r2 on ADRV9361-z7035 board
https://github.com/analogdevicesinc/hdl
for OS i m using Kuiper Linux
https://github.com/analogdevicesinc/linux
I have successfully run HDL reference design on vivado with ADRV9361…
According to the wiki the maximum throughput is 1066Mbps (not 1066MT/s), which would mean at a sample rate of 61.44MSps (max sample rate), DMA has absolutely no chance of streaming real-time.
Is this correct? Or is the DDR3 actually 1066MT/s and thus have…
Hello,
I am customizing my adrv9361-z7035 + fmc board and I wanted to know
What is the difference between doing my board configuration with ad9361 non-Os API or with AD9361 ParamInit?
Thank you,
Nicole.
I selected LOs frequencies as I did for adrv1crr-fmc reference design ( that is RF Bandwidth 50 MHz , Profile 1 2425MHz, Profile 2 2475MHz , dwell sample value 15000).
The above settings work correctly with Adrv9361-z7035+adrv1crr-fmc but not working…