Will ADRV9010 support DPD and CFR? Will there be a DPD version of ADRV9010 available in future?.
The user can refer to “ adi_board_adrv9010_JesdBringup “ API function in adi_adrv9010_daughter_board.c file. Take the link sharing mode with Framer 0 & Framer1 as an example. The JESD204 link sharing framer link bring up procedure in general follows the…
The user can refer to “ adi_board_adrv9010_JesdBringup “ API function in adi_adrv9010_daughter_board.c file. Take the link set up of De-framer 0 as an example. The JESD204 De-framer link bring up procedure in general follows the following steps on ADI…
What is the typical power consumption of ADRV9010.
ADS8 or ADS9 is required for the evaluation of ADRV9010. No other FPGA boards are supported.
What are the main difference between ADRV9010 and ADRV9026?.