adrv9009-iiostream from libiio/examples works. So I guess its just my code.
adrv9009-iiostream from libiio/examples works. So I guess its just my code.
Hello! I use adrv9009 + zcu706 of ADI company. I use tes provided on the official website to generate matlab script, and use matlab script to control the evaluation version and adrv9009, but the MATLAB script will report an error (2020b used by Matlab…
When I apply ADRV9009, the frequency hopping range is required to be from 600MHz to 6000MHz, the frequency hopping step size is 200MHz, and the frequency hopping interval time is required to be within 5ms. I have tested that only TX QEC and LOL are called…
Hello,
I would like to figure if ADRV9009 can send totally different IQ data on its 2 TXs. With IIO Oscilo I can send one single data file on every output.
I tried to use the iio_writedev comand like that : (the txt file comes from IIO Oscilloscope's folder…
Hi,I am using the hdl 'master' branch . And i am using no-os master branch. And I am using the project design for zc706 and EVAL-ADRV9008/9.
The signal power input to rx1 channel is -9 dBm to -4dBm.The agc index is around 0xfb ~0xe3.
I'm using…
Hello everyone,
we plan to investigate the performance of the ADRV9009 (and potentially the ADRV9002) under radiation conditions. We want to supervise especially the transcevier state through the SPI registers, specifically here the attributes that fall…
Hi,
I'm seeing the same issue described in this post.
Essentially running adrv9009 in fhm mode with mcs enabled. But sync is not achieved some of the time.
MCS works fine in non hopping mode.
I am operating through linux, and just calling the hop function…
Hi,
I'm working in on a custom board with ADRV9009, and continuous SYSREF from FPGA.
Sometime, FramerStatus is 0x27. SYNC pin is always 1. I haven't seen anything special at RX data from ADRV9009 to FPGA.
According to user guide, Bit 1: SYSREF…
Hi ADI,
I am currently using windows version of IIO oscilloscope with Xilinx ZC706 and no-OS. I have noticed that that the IIO has only 2 devices available-
axi_adc and axi_dac.
There are only 2 tabs/plugins available
debug and DAC data manager.
I have…