• RE: Can ADI's provide ADRF6850 debugging software for me?

    You can download the ADRF6850 evaluation board control software here: ftp://ftp.analog.com/pub/evalcd/ADRF6850/

    This software generates and controls the ADRF6850 registers through the SPI interface.

  • RE: ADRF6850 frequency setting

    Thanks for your reply sir,

    We are not using labview software to configure the AD demodulator, We are configuring ADRF6850 with stm Microcontroller and able to write and read registers from ADRF6850. The problem is we are not getting the correct LO frequency…

  • ADRF6850

    像ADRF6850之类的带有全差分放大器的的vocm管脚,大家一般使用都是默认使用电源电压的一半吗?

  • ADRF6850 GERBER Files

    Dear Sir/madam,

    Now we need gerber file for ADRF6850 IQ demodulator ic.This is required for our ground receiver project.Kindly send the gerber file ADRF6850.


    Thanks very much!


    Br,

    Wayne

  • I got a question about ADRF6850 & AD9265 interface circuit

    hi i'm sarah

    i'm looking for a making the Receiver

    i select the chip of ADRF6850 & AD9265

    so i need connection of ADRF6850(Receiver chip) & AD9265(ADC)

    ADRF6850 have interner iq demodulator so it can offer the baseband signal , and…

  • RE: How to use TESTLO Inputs of ADRF6850?

    H Sascha

    The ADRF6850 does not support using an external LO.

    Regards,

    Tim.

  • RE: Noise Figure ADRF6850

    The specified differential offset voltage on the baseband outputs of the ADRF6850 is +/-20 mV.

  • ADRF6850 baseband bandwidth

    Hello, we would know if the ADRF6850 max baseband bandwidth of 250 MHz in wideband mode is referred to each one of I or Q single outputs (and so the total available bandwidth in I/Q mode is 500 MHz) or it is referred to both outputs overall (i.e. the…

  • I use ADRF6850 encountered problems.

    1. Hello. I use ADRF6850 encountered problems:

    I use the microcontroller write control word,ADRF6850 was not able to lock to set frequency.

    But using ADRF6850_SPI_Rev2.vi debugging software, it can be locked to the set frequency .

    I have done this…