Hello, what would be the typical value for VCO_LDO for the ADRF6807 (at DECL1 pin) ? I measure 1.2V on the ADRF6807 eval board and would like to confirm this is a correct value. Thanks.
Hello,
I have the evaluation board of adrf6807, energized in the following way:connected 5v to VCC and 3.3v to 3P3V_FORCE, but when uploading the registers and then turn off the equipment.
I must have the configuration done again, the registers aren…
最新中文资料更新
中文数据手册
AD5204/AD5206: 4/6通道数字电位计
ADSP-BF592:Blackfin嵌入式处理器
ADL5545: 30 MHz至6 GHzRF/IF增益模块
AD5122/AD5142: 双通道、128/256位、SPI、非易失性数字电位计
ADP5050: 带四通道降压调节器和200 mA LDO调节器的5通道集成式电源解决方案
ADXL103/ADXL203: 精密±1.7 g/±5 g/±18 g单轴/双轴iMEMS加速度计
ADL5382…
Hello!
I'm using an ADRF6801 demodulator in combination with an ADRF6701 modulator.
I want to monitor junction temperatures of both chips, so the chips were configured to use the VPTAT temperature proportional voltage output at the MUXOUT pin.