• ADRF6780

    Dear Community,

    I am working with the Modulator ADRF6780, when I write and then read the registers sometimes is the value of the register not the  right value.

    I have switched of the parity functionality and at the end of the read or write bits is added…

  • ADRF6780-EVALZ

    Dear community, I have to work with the ADRF6780-EVALZ board and I have to connect to this board over SPI, but I cannot find a SPI Interface to connect the cable. Does somebody know ho I can do this?
    Best Regards,
    Iordan Pentchev.

  • ADRF6780-EVAL ACE program error

    Could anyone clarify and give me any advice?

    Part : ADRF6780-EVAL

    Testing of the ADRF6780-EVAL was completed in September 2021.
    But,
    ADRF-6780-EAVL does not work due to the update of the ACE program (November 2021 update_ACE 1.24.3095.1398).
    PC and ADRF6780…

  • ADRF6780 Eval board not recognized

    Hi,

    We have buy an ADRF6780-042654B. If the USB driver is not installed the Device Manager says the correct name:

    However once I install the driver the name changes:

    In both cases eval board is not recognized by ACE:

    I have tried in two computers…

  • RE: ADRF6780-EVAL ACE program error

    Could anyone clarify and give me any advice?

    Part : ADRF6780-EVAL

    Testing of the ADRF6780-EVAL was completed in September 2021.
    But,
    ADRF-6780-EAVL does not work due to the update of the ACE program (November 2021 update_ACE 1.24.3095.1398).
    PC and ADRF6780…

  • ADRF6780 Shield Enclosure Clearance Recommendations

    We are currently using the ADRF6780 in a design and are looking at clearance requirements for an RF shield enclosure.  Namely, do you have a recommended z-height clearance from this IC package to a metal shield lid?  We would like to keep our design as…

  • ADRF6780 LO inputs - DC or AC coupled?

    Hi,

    Hopefully an easy question.

    I am designing with the ADRF6780 and have a differential LO output from a LMX2594 to connect to it.

    Should the connection be DC or AC coupled?

    Many thanks, 

    Pete

  • ADRF6780 differential interface

    What is the performance penalty, if any, for substituting a balun for a 180 degree hybrid for the IF inputs and the RF outputs? Thanks in advance.

  • ADRF6780 DC Power Connections

    When using the ADRF6780 IQ Up-converter in IF mode without the RF detector is it necessary to add decoupling caps and supply DC power to VPBB, VPBI and VPDT?

  • ADRF6780 Absolute Max Input Levels?

    What are the IF and base band I/Q absolute max input levels for the ADRF6780? I don't see anything on the datasheet for this.

    Thanks,

    Steve