• RE: Load stability of ADRF6750

    Here's the output of the SAW on a power meter with no attenuation on the ADRF6750:

    And this is what it looks like with the ADRF6750 set to 1dB:

    And here's the ADRF6750 set to 0dB with an external DC-blocked 1dB attenuator between it and the…

  • RE: ADRF6750 Thermal Charactersitics

    The ADRF6750 Theta-JC is 2.4°C/W

    Regards,

  • ADRF6750 LOMON

    Hi,

    do you think it's feasible to use the LOMON port to feed the ADL5380 demodulator?

    Thanks a lot.

    Regards,

    Alberto

  • ADRF6750 divider didn't work

    Hi,

    I designed ADRF6750 b'd.

    When first time, I feed 10 MHz reference clock and 1200 MHz RF clock. It work very well.

    Now I want re-use this b'd for 54 MHz reference clock and 1200 MHz RF clock. But, it didn't work.

    "didn't work" mean…

  • ad9361的边界杂散问题

    请问ADI和各位大神,AD9361的整数边界杂散指标是多少啊?

    我以前用ADI的小数分频芯片如ADF4112、AD4350、ADRF6750等杂散都能控制在近-60dBc以下,现在用AD9361,参考源用50M,如果发送频率是50M的整数倍,如3.9G时,杂散指标很好,可达60dB以上,而发送频率为3.9001G时,就会在100K或200K或300K处出现杂散,有时只有40dBc不到,当频率偏移50M整数倍更多,超出环路滤波器带宽时,又会变小。请问这是AD9361的指标水平吗?

  • TAGS LIST: RF and Microwave

    HMC928
    HMC929
    HMC931
    HMC932
    HMC933
    HMC934
    HMC935
    HMC247G
    HMC538
    HMC-C018G
    HMC-C025G
    HMC-C053G
    HMC-C584G
    HMC7056G
    HMC7054G
    HMC7053G
    HMC7056AG
    HMC642G
    HMC642AG
    HMC643G
    HMC644AG
    HMC647
    HMC647A