• RE: ADRF6612 Lock Detect value when ext LO is used

    Hi Kevin

    Thanks for the update. We will be working on the schematic once we receive it. At the same time, we are working on why you obtain such behavior from the LOCK_DET pin.

  • RE: 关于ADRF6612

    This question has been closed by the EZ team and is assumed answered.
  • when the pll in adrf6612 is locked the muxout level is high or low?

    when the pll in adrf6612 is locked the muxout level is high or low?

    adrf6612内部锁相环锁定后,muxout管脚是高电平还是低电平啊? 手册给出是高电平是代表锁定,但是我的板子测试时是低电平锁定,请帮忙解答,谢谢。

  • RE: ADRF6612寄存器配置

    This question has been closed by the EZ team and is assumed answered.
  • RE: 关于ADRF6612请帮忙解答,谢谢。

    This question has been closed by the EZ team and is assumed answered.
  • RE: ADRF6612 GSM VCO frequency range

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: 请帮忙提供一份ADRF6612的寄存器设置,谢谢。

    This question has been closed by the EZ team and is assumed answered.
  • How do I enter loop filter components from the ADRF6612 eval board into ADISimPLL?

    I want to simulate the ADRF6612 eval board in ADISimPLL. How do I enter loop filter components from the ADRF6612 eval board into ADISimPLL? When configuring ADISimPLL with the ADRF6612 as the chosen device, I do not see a means to enter loop filter components…

  • RE: ADRF6620 EVAL board and software issue

    The reason that we used ANRF6612 instead was the tech support initially suggested that the ADRF6620 didn't have the latest version available.

     

    From: ADI Americas Tech Support <CIC.Americas@analog.com>
    Sent: July 22, 2016 8:16 AM
    Subject: RE…

  • RE: ADF4159 - Hardware and Software setup

    Hi !

    Thanks for the prompt feedback, please find attached the ADIsimPLL file (renamed as *.txt instead of *.pll) and the configuration file we use with ADF4158/9/69 PLL Software (version v4.10.6 July 2015)