Hi,
Unfortunately, the ADRF6602 registers are stored in volatile memory, and lose their programming once power is removed. Software must be initialized at power-up to place the chip in the desired state.
Thanks,
Darrell
Hi,
Unfortunately, the ADRF6602 registers are stored in volatile memory, and lose their programming once power is removed. Software must be initialized at power-up to place the chip in the desired state.
Thanks,
Darrell
你好,我现在调试芯片ADRF6602,5V供电,上电后电流大概0.27A。
问题1 是上电在端口LON,LOP测试初始振荡频率大概是在2.2G左右,当写入控制字后,振荡频率变为3.4G左右,电流变为0.16A,根据内部LO的频段1550-2150MHz(这个频点是经过VCO 2 分频的吗?),当我重新断电后,上电频率也是2.2G左右,但是写入控制字后就没有振荡频率了,电流也变为了0.05A,经测试,2脚电压为0,(前后两次写入的程序相同),上诉两种情况都会出现,我曾将MOUXOUT引出参考信号…
Dear Sirs,
since four years we used the ADRF6602 as a down-converter. LO freq. = 1605,425MHz. We never changed the hardware (PCB) and also the software was never changed. The converter worked fine the hole time. Now - arround four years later a problem…
从ADI经销商那买了个ADRF6602的评估板套件,用套件中自带的USB线将评估板和PC机链接后出现安装提示,
我选了默认的自动安装,点下一步,告诉我安装不成功。
我在资源管理器中看也是没安装成功
现在我没有办法使用评估板套件,显示我的评估板没有连接成功。
联系了经销商,让我拍开发套件的照片过去;联系ADI的客服,让我电脑截图,发邮件。
1天就这么过去了,也没个人能告诉我问题出在哪?
请问专家对应的驱动程序我应该到哪去下载?