• about the power ADRF5160

    Can it be operated at 200 MHz-512MHz? Power Range Peak 44dBm,Pulse width 4ms,Duty cycle max 10%

  • ADRF5160

    What is the minimum operating frequency other than the datasheet?
    Can it be operated at 20 MHz?
  • Question about ADRF5160

    Hello,

    I look forward to your reply to the following questions.

    With RFC and RF1 in conducting state, input a +40 dBm signal from RFC.

    If RF1 is open and the power is totally reflected, can the ADRF5160 fail?

     

    With RFC and RF1 in conducting state, a…

  • ADRF5160

    Hello,

    ADRF5160 is rated for 88W peak power during off position. In my design, this part will see 100W peak power during OFF position? Is there any risk using this part which is only rated for 88W? Has Analog devices conducted any test with 100W peak…

  • RE: ADRF5160 unexpected I.L

    Marked as answered due to lack of reply

  • the power reflections from the RFC pin of ADRF5160 during switching

    Hi,

    This technical query is regarding the product ADRF5160-EVALZ-ND (evaluation board for RF switch ADRF5160).

    We Intend to use the switch as described below.

    1) an input signal (generated from a signal generator in our case) is applied at the RFC terminal…

  • RE: About the HMC646 Power Handling

    Hi Sinan,

    We broadcast in 2.5ms with a 1.5ms pulse width. In other words, 100W (peak power) is open only in the 1.5ms region.

    I will consider ADRF5160, thanks for recommendation. 

    BR,

    Gozde

  • RE: High and Medium Power RF Switches (70MHz-6GHz)

    Hi,

    ADRF5130, ADRF5132, ADRF5160 are our high power (>20 W peak) SPDT switches in SOI process. Unfortunately none of them could handle the power level in wide frequency range of your application.

    Best.

  • TAGS LIST: Switches/Multiplexers

    AD8104
    AD8105
    AD8106
    AD8107
    AD8108
    AD8109
    AD8110
    AD8111
    AD8112
    AD8113
    AD8114
    AD8115
    AD8116
    AD8117
    AD8118
    AD8175
    AD8176
    AD8177
    AD8178
    AD8186
    ADV3200
    ADV3201
    ADV3202
    ADV3203
    ADV3205
    ADV3224
    ADV3225
  • RE: Query

    This part is EAR99. The attached RFIC selection guide lists the ECCN codes for all of ADI's RF products.

     PDF