• Connecting two ADRF5026 in series

    When connecting two ADRF5026-EVALZ MPN in series, VDD started drawing more current and both the switches went to OFF(Isolation) state. And its in OFF state since then, I'm thinking something has damaged the switches. What went wrong? or Is it okay…

  • ADRF5026 RFx pin with TVS diode

    Hi ADI expert,

    Since QC engineer is sorting NG components and found that some component status showed different than good one.

    When use DMM diode function to measure pin8/RFC, some showed open status, but some showed forward bias with ground or VDD.

  • RE: ADRF5026 insertion and return loss at 125 degree Tcase

    Hi ZWang

    I was talking about the Rdc of the path RF1/RF2 to RFC  inside the ADRF5026

    thank you

    Ken

  • ADRF5026 footprint

    The ADRF5026 datasheet shows layout pad dimensions in Figure 21 of 8 x 10 mil.  The Ultra Librarian layout for this part shows pad dimensions of 10 x 12 mil. 

    www.analog.com/.../symbols-and-footprints.html

    Which footprint do you recommend?

    Thank you.

  • ADRF5026-EVALZ

    I would like to know what the model number is for the SW Microwave 2.4mm Edge Launch connector used on the ADRF5026 eavluation board (ADRF5026-EVALZ).  Specifically, we would like to populate the THRU Cal without borrowing connectors from the switch.  Thank…

  • ADRF5026, ADRF5044 Control Signal Application Relative to Vdd

    For part numbers ADRF5026 and ADRF5044, I may not be able to control the timing of when control signals inputs get applied relative to the application of Vdd as described in their datasheets.

    I understand if I apply a logic high to the switch control…

  • ADRF5044&ADRF5026 switches not working

    My name is Neelima, I am working as a design engineer in UTS R&D domain.

    We recently Design one R&D PCB with ADRF5044 SP4T switch along with the ADRF5026 SP2T switch Interface.

    Yesterday, We tested our designed board and we didnt get the expected…

  • ADRF5044 and ADRF5026 Switches are not working!!!!

    My name is Neelima, I am working as a design engineer in the UTS R&D domain.

    We recently Design one R&D PCB with ADRF5044 SP4T switch along with the ADRF5026 SP2T switch Interface.

    Yesterday, We tested our designed board and we didnt get the…

  • ADRF5026 DC level at RF ports

    Hi,

    For ADRF5026, no DC blocking capacitor are required at the RF ports, but what is the maximum admissible DC level at RF ports without stress?

  • ADRF5020 &ADRF5026 compatible issues

    Currently we have a new project design in ADRF5020 and will hope ADRF5026 footprint compatible with ADRF5020 after the part release.

    Could you help me to check difference between the ADRF5020 & ADRF5026.

    Pad size & pitch is as same?  

    Thank you…