Hello dear colleagues!
Could you send me a footprint for ADRF5024?
Thanks.
Sincerely,
Kirill
Hello dear colleagues!
Could you send me a footprint for ADRF5024?
Thanks.
Sincerely,
Kirill
Hi,
I have a question on the power handling of reflective switches, such as ADRF5024
https://www.analog.com/en/products/adrf5024.html
I would need it for an application where an high reflection coefficient (ideally, 0dB for S11) is required in the "off…
Hello!
We are designing a DAC module based on the AD9173. You can see the desired schematics on the picture below. We need frequencies on the output to be from 10 kHz all the way up to 6 GHz.
We understand that output of the DAC needs to be terminated…
Hi,
I am looking at a few ADI RF switches, ADRF5024, ADRF5025, and ADRF5047. I notice the VDD, VSS, and CTL voltage/current specifications for these switches are all very similar except the ADRF5047 has specified VCTL low of 0V to 1.2V and VCTL High…
Do you need to have both outputs operating at the same time?
If not, you could piggy back 2 SPDTs. As such:
To answer your question: we specify switching characteristics for a typical part in the datasheet (Ton, Toff, Trise, Tfall). There may be up t…
Part 1:特色产品
AD9164:16位、12 GSPS、RF DAC和直接数字频率合成器
该DDS由一组32个32位数控振荡器(NCO)组成,各带相位累加器。与100 MHz串行外设接口(SPI)和快跳模式配合使用时,支持相位相干快速跳频(FFH)和几种模式以支持多种应用。
系统方案精选 APM
应用笔记 APPLICATION NOTE
技术文章 TECHNICAL ARTICLE
模拟对话 ANALOG DIALOGUE
…AD8104 |
AD8105 |
AD8106 |
AD8107 |
AD8108 |
AD8109 |
AD8110 |
AD8111 |
AD8112 |
AD8113 |
AD8114 |
AD8115 |
AD8116 |
AD8117 |
AD8118 |
AD8175 |
AD8176 |
AD8177 |
AD8178 |
AD8186 |
ADV3200 |
ADV3201 |
ADV3202 |
ADV3203 |
ADV3205 |
ADV3224 |
ADV3225 |