I want to know exact phase of RFC-RF1 & RFC-RF2 because i will connector RF1 and RF2 with other RF lines.
Connector - RFLINE -RFC - SPDT - RF1 - RFLINE
When chip is connected like above, i want to know highlighted phase.
Thanks
I want to know exact phase of RFC-RF1 & RFC-RF2 because i will connector RF1 and RF2 with other RF lines.
Connector - RFLINE -RFC - SPDT - RF1 - RFLINE
When chip is connected like above, i want to know highlighted phase.
Thanks
Dear Sir/Madam,
I have checked the wafer fabrication and it state BiCMOS.
I would like to find out the if ADRF5021 (SPDT) is based on BiCMOS SiGe fabrication?
thanks
Regards,
Nick
Hi All,
I am intending to use ADRF5021 in one of our new designs. I have a 30GHz signal that will be fed to the RFC port, two loads will be connected to RF1 and RF2 and a control logic will switch between the loads.
The rise and fall time of my signal…
Hi,
Does the ADRF5021 have any internal pullup or pulldown resistor?
I don't see any mention of this in the datasheet, but if I missed it please point it out to me.
Want to verify if its ok to leave pin floating (only in case of pulldown resistor…
Does anyone know what the lumped capacitance is for the ADRF5021 RFC and RF1/RF2 pins?
Would be for the shunt and series equivalent input capacitances; we use dc blocks at the input but
we're needing to understand the effecr of the ADRF5021 switch on…
Q.
Many of the RF and Microwave SOI switches require dual voltage supplies (VDD and VSS). Which of these may be operated with only a single positive supply (VDD)?
A.
Certain switches from the SOI portfolio may be operated using only a single positive…
我公司预使用ADI两个开关产品,一组:ADRF5044/ADRF5045 二选一;二组:ADRF5020/ADRF5021二选一;现想咨询一组和二组开关可否级联使用?谢谢