• RE: ADR444 reference design for noise reduction?

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: how is the sensitivity and potential of the trim pin of adr444

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • ADR444 Incorrect Output Voltage

    I am trying to use the ADR444 as a 4.096V reference for the ADAS3023, using the AD8031 as a buffer, as suggested on the ADAS3023 data sheet.  The ADR444 is giving about 4.3V, which is dropping to 4.2V after the AD8031.  Both of these are operating off 5V…

  • ADA4841-1 0.1Hz to 10Hz noise

    Hello, 

    Are there any information available for ADA4841-1 about the voltage noise density vs. frequency in the range 0.1Hz to 10Hz?

    If not, are there information available about the 0.1Hz to 10Hz voltage noise (peak-peak)?

    I will use the ADA4841-1 as a…

  • ADAS3022 recommended ADC driver, external reference and reference buffer options

    What are the recommended ADC driver, external reference and reference buffer
    options?

     

    The ADAS3022 datasheet recommends the ADA4841 and AD8031 as ADC driver (to
    drive auxiliary input pair - AUX±) and reference buffer, respectively. Other …

  • ADAS3023: Recommended ADC driver, external reference and reference buffer options

    What are the recommended ADC driver, external reference and reference buffer
    options?

     

    The ADAS3023 datasheet recommends the ADA4841 and AD8031 as ADC driver (to
    drive auxiliary input pair - AUX±) and reference buffer, respectively. Other

  • recommended ADC driver, external reference and reference buffer options?

    What are the recommended ADC driver, external reference and reference buffer
    options?

     

    The AD7961 datasheet recommended ADC drivers are the two single-ended op amps
    ADA4899-1 and AD4897-1 or differential amplifier ADA4932-1. The low-noise,
    low-power…

  • RE: I need IBIS model for ADM1270

    Hi Priyanka,

    IBIS models are only used for modelling digital pins. Since the ADR444 is a voltage reference with no digital pins we do not provide an IBIS model for this product.

    Regards,

    Rob

  • CN0143 - Mistake in Figure 3

    The output of U4 (the ADR444) is not connected; what is currently drawn to the NC pin (No Connect) should be drawn to VOUT.

    [Edited for clarity]

  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…