• related components to ad5933?

    hello

    I 'm new in electrical engineering and I want to know the necessairy components to work with ad5933  I mean that is an external clock necessairy to work with ad5933 and adr433 is also important?

    thanks for replying.

  • [征文] IN118的基准源用AD的芯片,上面写着D6B,困饶我很久了 AD5312


    这个芯片(AD9833)的名字我猜的,可忽略看,如果是这个芯片,左看右看也不知是干吗呢?

  • REF input of AD5449

    Hi:

    I want to use AD5449 in my design. The REF pin must be provided the external reference input, while the input resistance of REF pin is  11K ohm. The datasheet suggest to use ADR*** to generate the reference input, like ADR06(output current is 10mA…

  • AD5933 with big errors

    experiment with sample circuit, voltage source ADR433, resistor connected between VOUT and VIN  1kΩ and the feedback resistor  1kΩ to calibrate the gain factor.internal crystal oscillator ,excitation frequency 30Khz , 1Vpp.

    1K
  • ADI芯片辨识、型号查找

    看看截图:

  • RE: AD5933 setup

    Hi Miguel,

    I am sorry about the mark in the Capacitor only position. I have always been running simulation with resistance and never changed that value. By the way, also with the mark in Resistance only position, the results stay as the same as the ones…

  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…