• I would like to use an ADR3450 in order to build a 300mA, high precision, 5V voltage regulator.

    I would like to use an ADR3450 in order to build a 300mA, high precision, 5V
    voltage regulator.
    How can use it, if the maximun input voltage is really 5.5V (6V in absolute
    maximum ratings)?

     

    The ADR3450 would need an input voltage of 5.2 to 5.5V. Its…

  • RE: ADR3450, increase output capability

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADR3450ARJZ-R7

    Hello, Thank You for your reply.

    I have already exchanged ADR3450 with REF195 in my design and managed to find space for it on PCB. REF195 will suit me better I think. I would appreciate Your opinion.

    Best regards,

    Tom

  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…
  • RE: Typical standby power

    Hi, sindhu.

    ADR293 does not have any disable and is not recommended for newer designs. Use ADR3450, ADR3550 for new designs. AD8041 has 1.7mA when disabled for 5V operation. Please see spec tables of the datasheet - http://www.analog.com/static/imported…

  • 【在线研讨会】电压基准源的产品及选择

    基准电压源是当代模拟集成电路极为重要的组成部分,它为串联型稳压电路、A/D和D/A转化器提供基准电压,也是大多数传感器的稳压供电电源或激励源,几乎在所有先进的电子产品中都可以找到。在近期的在线研讨会《电压基准源的产品及选择》中详细介绍了基准电压源的分类及工作原理和各类基准源的性能指标及主要的应用场合以及ADI的基准电压源的设计开发规划、产品优势以及对客户应用的价值所在。

    本期研讨会的回放请点击:http://www.elecfans.com/d/908063.html

    附件是本期研讨会的讲义,供大家下载并学习…

  • 问题: ADI最新中文资料(2011年4月)

  • 重磅推荐!ADI 锂离子电池测试设备解决方案

    能源消耗始终是全球需要面对的普遍问题。市场期待更安全、 更干净、更高效且更低成本的电源。由此催生了混合动力和电 动汽车、太阳能和风能技术这些解决方案,它们共同的关键因 素是锂离子电池。随着这三大领域迅速增长,锂离子电池在节 能方面将发挥越来越重要的作用。

    锂离子电池制造程序非常复杂,包括电极生产、堆叠结构、单 元装配。之后还要执行电气测试,激活电池功能并评定电池容 量,确定额定性能和价格。为了在锂离子电池制造过程中执行 这些电气测试,需要高度集成、高效率和高精度的测试设备, 这也正是 ADI 公司基于…

  • ADI公司解决方案通报—放大器IC

    目录

    • 差分放大器采用单电源驱动1.8 V ADC
    • 电流检测放大器实现最大1μV/°C的失调漂移性能
    • 经过测试的电路设计
    • 热电偶放大器简化设计
    • 放大器IC选型指南
    • ADC驱动器提供快速压摆率
    • 同类最佳的电压反馈型放大器
    • 输出驱动器增强灵活性和性能
    • 差分放大器驱动184 MSPS SAR ADC,接受±10 V输入
    • 高分辨率、零漂移电流检测放大器
    • 适用于高精度设计的微功耗基准电压源
    • 精密放大器针对低功耗、宽电源电压范围应用而优化