• ADR3425 fan out recommended circuit

    Hi,
     
    The ADR3425 2.5v reference voltage must be provided to AD7490 * 10pcs ADCs. Is there a recommended circuit?
     
    Thank you
  • AD7190读数误差问题

    使用AD7190进行电压测量,AN1伪差分输入模式,采样速率为20Hz,基准电压为2.5V由ADR3425提供; 

    输入11mv时,AD7190测得电压为8.4mv; 请问时什么原因造成的?

  • RE: AD7490 Sampling Rate & Artifacts

    Hi ,

    Thanks for the response. We're using the ADR3425 for REFIN. Please see the attached image. Just a note about the schematic: the AAFx components are hierarchical blocks containing a programmable filter circuit.

  • RE: Use of TL431 for voltage reference of AD7683

    FormerMember
    FormerMember

    I would not even consider the TL431 with a 16 bit ADC;  you are just throwing money away.

    The TL431 is a commodity reference, with 50 ppm/C tempco.  So after your temperature

    changes by 10 degrees, you have less than a 14 bit system.   There is a noise…

  • AD7192输出数据错误

    使用AD7192,伪差分单极性接入1.5v信号,AINCOM接GND,单通道读取数据,有四十位4177066232。程序跟外围接线图如附件,想请专家帮忙看看我硬件还是程序出了问题。REF用的ADR3425.

  • RE: AD719x reference buffer amplifier?

    FormerMember
    FormerMember

    Oliver,

    Why do you say the reference input draws high peak currents?  I didn't see that in the d.s. and it's

    a sigma-delta, not a SAR??

    The eval board uses an ADR421, so that or an ADR43x should be fine.  I like the 43x family

    because you can…

  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…
  • RE: REF192 dropout

    FormerMember
    FormerMember

    NA,

      Fig 19 is for the REF195, which is similar to the REF192.  If you look at fig. 20 in the d.s.,

    the pass element is a PNP, so Vce(sat) is probably less than 0.3V, so you should not have

    any problem.  However, why use the REF192, which is more than…

  • RE: ADR3412 voltage reference

    Hi TrezTan,

     

    Here is the answer I got "We only have a spice model for the ADR3425 (the 2.5V output version of this family). It is used as an example
    of behavior. Other voltages behave similarly." The spice models are available at:

    SPICE Models…

  • RE: AD623 output need operation time for stable output?

    FormerMember
    FormerMember

    Howard,

    What are the red and blue traces?  Which 623??  top or bottom?

    Everything has a tempco.  If you want very stable operation, you need to use resistors that are 5-10ppm/C tempco,

    and get rid of the junk op amp, LM2904.  Do not use a dual.  You did…