Hi ,
could you please let me know the Absolutist Maximum rating of Vout pin .
I would like to know this because there are case when the input falls below the Vout and Vin < Vout (Capacitor).
Thanking you
With best regards and wishes
Hi ,
could you please let me know the Absolutist Maximum rating of Vout pin .
I would like to know this because there are case when the input falls below the Vout and Vin < Vout (Capacitor).
Thanking you
With best regards and wishes
Hi,
What is the operating system you are using? Are you using an evaluation board or your design already?
Can you try the installer in the attached file? The installer should include the software: I2CWSD.
Have you initiated the download…
LT1460 |
LTC1258 |
LT1021 |
LT1027 |
LTC1798 |
RH1021-10 |
RH1021-5 |
RH1021-7 |
LT6660 |
LH0070 |
LTC6655 |
AD2700 |
AD2702 |
AD584S |
REF01S |
REF05S |
REF10S |
REF43S |
REF02S |
AD1582 |
AD1583 |
AD1584 |
AD1585 |
LT1019 |
LT1236 |
LTC6652 |
REF02… |
PDFADuC7023 Eval board Programming.zip
See pages 3 & 4 of the attached document for details on how to mass erase the flash on the evaluation board.
Regards,
Mike
As in the data-sheet specified - a external reference should be in the range from 0.625V to AVDD.
As can be expected the output current to the Vref input isn't that big - so as a guidance you can start with the ADR291 specifications- we placed on…
PH计设计的主要考虑因素有: 稳定性、分辨率、低功耗。结合上面提供的咱们ADI的解决方案,看看如何满足这些需求:
多数pH计提供3.位的分辨率,这意味着16位Σ-Δ ADC即足够。某些实验室pH计的分辨率可能高达5.位,此时应当使用AD7793等。24位Σ-Δ ADC和低闪烁噪声放大器ADA4505-2/AD8626。
仪器仪表的一大趋势是小型化和便携化,这对低功耗设计带来挑战。上表中每个类别下的产品中都有低功耗器件。例如:ADA4505-2/AD8626、ADR291、AD7792/3、ADuCM361…
土壤酸碱度测量仪
随着生产和生活越来越工业化、现代化,环境对我们人类的影响问题也变得很突出!
大家认识到加大力度保护空气、水、土地、森林等宝贵资源刻不容缓!
民以食为天,粮食是宝贝,生产粮食的土地是宝中宝!现在的农业生产由于大量使用化肥和农药使得土壤的
酸碱度偏高或偏低,部分改变了土壤的结构,不利于农作物的生长,导致了粮食和庄稼的减产。
传统的PH测量采用化学试纸办法,效率低,测量误差较大;同类的电子产品稳定性不太好,精度不高,功耗大,功能单一。
因此我想设计一款能测量土壤酸碱度的仪器…
这是第二篇有关分光光度计应用的文章。在第一篇文章中——ADI双光束分光光度计解决方案(http://www.analog.com/media/cn/technical-documentation/apm-pdf/adi-dbs-solutions_cn.pdf),我们讨论了应用、工作原理、电路架构和设计考虑因素。本文将介绍ADI公司的相关新演示系统和产品。
下载ADI灵活全面的系统解决方案及主要产品简介请点击:http://www.analog.com/cn/design-center/landing…