• RE: ADR280 .1 - 10hz voltage noise

    This question has been assumed as answered either offline via email or with a multi-part answer. This question has now been closed out. If you have an inquiry related to this topic please post a new question in the applicable product forum.

    Thank you,
  • RE: ADuC7060 and RTD_PieceWise_Linearization.zip ?

    Hi,

    The software example should work with the ADuC7060 evaluation board. The evaluation board uses a 2-wire RTD, but you can use the schematic of the evaluation board and the software example as a reference for a 4-wire RTD. I have attached the schematic…

  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…
  • RE: AD9833 Need +/- Vout and 50/60Hz

    Hi,

    Answering your questions:

    1) No that is a pin for decoupling to ground for noise/stability reasons.The AD9834 has the reference input /  output option - however for 1% tolerance I would advice using an external reference. The ADR280 or the ADR512…

  • RE: How to measure negative temperatures with a thermocouple on a battery powered device.

    Harry, yes my apologies it was meant to read ADR280.  I don't understand how the shunt reference IC's work.  Is it just a voltage supply with a series resistor that regulates the current into the diode?

    Yes I was referring to the AD8495.  If we…

  • RE: AD5930/32 Suitability

    Hi Dave,

    That should have read "It was not calculated using external". I have updated the preceding post also and removed the attachment.

    The data in the attachmenet  was to state:

    For the AD5930 with external precision 200Ohm resistor.

  • RE: About CF pulse of ADE7953

    Hi Dlath

    this schematic which i use

    I have a microcontroller quartz 6 MHz increments and in 3.57 MHz increments ADE does this affect you?

    Yesterday I calibrated with the ADE  7953 development board there is also jumping СF pulse? how to understand…

  • AD7608, AD7609: Schematic and PCB prints

    EVB schematic and layout files

     

    Please find the attached schematic, this version is provided by our product
    line engineer.

  • Looking for schematics for ADE7816

    Hi guys!

    Looking to use your UG-370 manual as a guide to using the ADE7816 for an AC meter for a microgrid project we are designing. However, the UG-370 user guide is too blurry to read (pages 13-15). Do you have readable copies of those schematics?

  • ADI芯片辨识、型号查找

    看看截图: