• ADR125: Output Capacitance

    Output Capacitance:
    The data sheet advises to add 10uF capacitor to inprove load response.

    Can I use also Ceramic capacitors without stability issues?

     

    Basically, having a large capacitor at the output, limits the rise time,
    prevents overshoots…

  • AD8657制作4-20mA电流环路发送器

    对于下面这个电路有点不是很明白,来自AD8657datesheet。图中Rsense电流时怎么分析的,R3和C1是起什么作用的,ADR125的GND和右下方的地的区别,求指导,谢谢!

  • What amplifier would you recommend for a low power  4mA to 20 mA  current loop transmitter application?

    For low power application that requires RRIO and greater than 5V supply, I would recommend the AD8657 due to its low supply current of 22 uA per amplifier. The AD8657 is a 18V, micropower, rail-to-rail RRIO amplifier optimized for low power and wide operating…

  • ADI芯片辨识、型号查找

    看看截图:

  • 放大电路设计必备宝典——论坛问答精华帖汇总

    ADI中文技术论坛开放以来,以“48小时快速解答技术问题”的专家团队响应机制受到中国工程师的热烈关注,注册用户持续增长,提问尤其踊跃。2013年底,美国新传播研究协会(SNCR)授予ADI技术支持论坛2013年度卓越成就奖!

    ADI中文技术论坛不仅为工程师提供技术咨询的窗口,还为大家的经验分享交流提供了一个宝贵的平台:

    • 这里累积了上万条工程师在实际设计中的技术问题及专家解答,这些来自设计实践中的技术问答是工程师们的设计参考宝典;

    • 这里还累积了上千条工程师的技术分享帖,是最直接、最给力的干货…