• ADR06 capacitive load

    Hello

    One of my customer is considering ADR06.

    The capacitive load would be 4uF. Can ADR06 drive it?

    Should they use buffer amplifier?

    If you have advice, it is helpful.

    Regards,

    Shumpei

  • 精密基准电压源芯片中的“初始电压精度”是什么意思?例如ADR06的初始精度:±0.1%

    精密基准电压源芯片中的“初始电压精度”是什么意思?例如ADR06的初始精度:±0.1%

  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…
  • AD7997 inconsistent conversion results, front end filter assistance

    I'm working on a design that includes the AD7997, the ADCMP393 and the TI LM2902 and am seeing inconsistent and inaccurate voltage reads from the AD7997.  I am trying to determine how to rectify this and produce stable and accurate reads from the AD7997…

  • REF input of AD5449

    Hi:

    I want to use AD5449 in my design. The REF pin must be provided the external reference input, while the input resistance of REF pin is  11K ohm. The datasheet suggest to use ADR*** to generate the reference input, like ADR06(output current is 10mA…

  • ADR03 Vout adjustment range

    Hi All,

    One of my customers has one problem with ADR03 output adjustment range.

    Part of his circuit schematics is attached.

    As shown in the schematic, Vout adjustment circuit is almost the same as shown in the data sheet, Figure 35.

    He said that the…

  • Is ADP2291 working as expected in the datasheet or its examples are fail?

    Hello Everyone,

    Im working on a battery charger circuit. I set completely the figure-22 and the figure-23 in the datasheet. So more than hundred try and later than weeks. The circuits are not working as expected. This part is important "The circuits are…

  • ADI芯片辨识、型号查找

    看看截图:

  • Daisy chain issue with AD5415

    If you are using or plan to use the AD5415 12-bit DAC chip in a daisy-chain configuration, you need to read page 20 of the marked up data sheet attached.  If you are using the SDO output of even a single AD5415, then you also need to see the erratum marked…