• ADR03 Vout adjustment range

    Hi All,

    One of my customers has one problem with ADR03 output adjustment range.

    Part of his circuit schematics is attached.

    As shown in the schematic, Vout adjustment circuit is almost the same as shown in the data sheet, Figure 35.

    He said that the…

  • AD5725 VREFN oscillation

    I'm using the AD5725 operating with the following input ranges : +/- 5V , +/-10V and any combination in between that doesn't violate the operating condition of VREF. 

    Since I'm using the +/-10V reference, I placed a 0.22uF bypass capacitor at inputs…

  • RE: Queries about AD5445 EVB

    Hi,

    Apologies for the delayed response. The software for the EVAL-AD5445SDZ is designed for a single write/read of the part. It does not have the waveform generator capabilities. The sentence "The software offers a waveform generator" is a typographical…

  • TAGS LISTS: Voltage References

    LT1460
    LTC1258
    LT1021
    LT1027
    LTC1798
    RH1021-10
    RH1021-5
    RH1021-7
    LT6660
    LH0070
    LTC6655
    AD2700
    AD2702
    AD584S
    REF01S
    REF05S
    REF10S
    REF43S
    REF02S
    AD1582
    AD1583
    AD1584
    AD1585
    LT1019
    LT1236
    LTC6652
    REF02…
  • Setting the full scale current output of AD5426

    Dear friends, 

    We are trying to design a 125kHz bipolar square waveform generator to communicate with a old digital computer. Its a form of BPSK type digital signaling.

    We shall connect the AD5426 thru a SPI bus to the uC, and will be using ADR01 for the…

  • ADI芯片辨识、型号查找

    看看截图:

  • Series or Shunt Voltage Reference for AD5546

    Hi I am following AD5546 evaluation board schematic for my design. But I need a reference of +12V to generate 0 to +12V for my application. But I could not find any fixed higher voltage references to replace the +10V ADR01BKSZ used in the board. I have…

  • Daisy chain issue with AD5415

    If you are using or plan to use the AD5415 12-bit DAC chip in a daisy-chain configuration, you need to read page 20 of the marked up data sheet attached.  If you are using the SDO output of even a single AD5415, then you also need to see the erratum marked…