• ADPD2211 active sensor area

    Where could I find any information about ADPD2211 active sensor area? Unfortunetely, there are no such data in the datasheet.  

    This information very important to optical design and it was suprise from a photos of this sensor that photodiode does not take…

  • ADPD2211 Mechanical Drawing

    Hi ADI team,

    Do you have mechanical drawing of IC ADPD2211, which shows orientation of photo diode sensor.

  • ADPD2211 light reflections

    Using ADPD2211 with 3 LED wavelengths, 630, 700, 810nm.  Detector is physically isolated with only 1 hole over the PD sensor. When measuring light levels the outputs varies when the current levels are constant.  Can reflected light be sensed by the PD?…

  • ADPD2211 The Best Mechanical Design

    Dear All:

    I want to Know ADPD2211 photo diode best window area on the mechanical have any dimension can provide to me refer.??

  • EVALZ-ADPD2211 size and senser position

    I am FAE in Japanese distributor.

    Our customer asks the size of EVALZ-ADPD2211 and sensor ( photo diode) position in the evaluation board.

    Please see the attached material and answer the X1,X2,Y1 and Y2.

    Best regards

    N.Kokubo

    EVALZ-ADPD2211.pdf

  • ADPD2211可以检测光纤内的光强度吗?

    ADPD2211作为光传感器,光波范围包括850nm光纤传导的波长,如果把光纤与ADPD2211衔接,就可以检测光纤内部的光强度,扩展了其应用范围,应用前景广阔。这种设想能否可行?请专家、坛友给予指导意见。

  • RE: Drawings or table of sensor positions and dimensions for ADPD2211, ADPD2212, ADPD2214

    Hi Moritz,

    I am sharing the drawings for the photoactive area for all three products below.

    This is ADPD2211:                     

    This is ADPD2212:               

    This is ADPD2214:                          

    Regards,

    Yigit

  • TAGS LIST: Optical

    AD800
    AD803
    AD807
    AD808
    ADN2804
    ADN2805
    ADN2806
    ADN2807
    ADN2811
    ADN2812
    ADN2813
    ADN2814
    ADN2815
    ADN2816
    ADN2817
    ADN2818
    ADN2819
    ADN2855
    ADN2905
    ADN2913
    ADN2915
    ADN2917
    ADL5315
    ADL5317
    LTC5100
  • RE: Which specific ADPD221x product is best for my application or design?

    The four ADPD221x products each have different potential applications.

    • The ADPD2210 is a standalone current amplifier, which takes any current source up to 10 µA as an input and sources 24x the input current on its output while adding very low noise…
  • 7月重点推荐,你最关注啥?

    1)宽带RF收发器AD9371

    http://www.analog.com/cn/products/rf-microwave/integrated-transceivers-transmitters-receivers/wideband-transceivers-ic/ad9371.html

    AD9371是一款高度集成的宽带RF收发器,提供双通道发射器和接收器、集成式频率合成器和测试和数字信号处理功能。IC提供FDD和TDD应用中3G/4G微和宏基站设备所需的灵活高性能和低功耗组合。该器件的工作频率范围为300…