• ADPD2210 in low light application - how to deal with 240 nA static bias

    Helllo,

    I am kindly asking advice on the following matter:

    We are considering to use the ADPD2210 as front-end for a photodiode in a very low light application. The

    expected photo-currents are in the range of 1-1000 pA.

    Since the ADPD2210 always exhibits…

  • ADPD2210 Interfacing with TIA

    Hi,

    I have an existing photodiode design which utilises a single supply TIA made from an ad8615. The metal can of the PD is hooked up to a reference voltage of 2.5V, as well as the non-inverting input of the amp. The other pin of the PD goes to the inverting…

  • TAGS LIST: Optical

    AD800
    AD803
    AD807
    AD808
    ADN2804
    ADN2805
    ADN2806
    ADN2807
    ADN2811
    ADN2812
    ADN2813
    ADN2814
    ADN2815
    ADN2816
    ADN2817
    ADN2818
    ADN2819
    ADN2855
    ADN2905
    ADN2913
    ADN2915
    ADN2917
    ADL5315
    ADL5317
    LTC5100
  • How to put LEDs on eval-boards of ADPD221x

    I bought eval boards of ADPD2210, 2211, 2212 and 2214.

    In order to test it for heart rate monitoring, I have to put an LED. 

    Can recommend and suggest LEDs that can be mounted on this board? or any tricks to put LEDs on these tiny boards?

    (Please don…

  • RE: Which specific ADPD221x product is best for my application or design?

    The four ADPD221x products each have different potential applications.

    • The ADPD2210 is a standalone current amplifier, which takes any current source up to 10 µA as an input and sources 24x the input current on its output while adding very low noise…
  • 7月重点推荐,你最关注啥?

    1)宽带RF收发器AD9371

    http://www.analog.com/cn/products/rf-microwave/integrated-transceivers-transmitters-receivers/wideband-transceivers-ic/ad9371.html

    AD9371是一款高度集成的宽带RF收发器,提供双通道发射器和接收器、集成式频率合成器和测试和数字信号处理功能。IC提供FDD和TDD应用中3G/4G微和宏基站设备所需的灵活高性能和低功耗组合。该器件的工作频率范围为300…

  • 智能可穿戴医疗保健设备解决方案

    先呈上完整资源包的下载链接:

    http://h.analog.com/CN-APM-WEARABLEff

    智能可穿戴医疗保健设备及典型架构

    可穿戴医疗保健设备可定义为能够自主监控或支持特定医疗功 能的无创式系统。(可穿戴的国家标准正在制定中) “可穿戴”一词说明该设备要么是直接佩戴在人体上的设备, 要么是一件衣服,并且具有适当的设计,支持其用作可穿戴配 件。广义上讲,这要求该设备具有极小的尺寸和重量,功能自 主,自备电源,易于使用,而且穿戴舒适。

    智能可穿戴医疗保健设备有多种类型,如腕带…

  • 重磅推荐!ADI 体外化学分析仪解决方案

    最新解决方案已上线,点击:http://h.analog.com/CN-VC-ANALYZER-ff?ADICID=SOME_CN_P114971 下载完整文档

    体外化学分析仪的典型架构

    生命科学与医疗仪器仪表包括各种不同的系统,比如体外化学 分析仪、流式细胞分析仪、输液泵、透析设备、呼吸器、导管 等设备。体外化学分析仪利用许多电化学和光学技术来分析血 液、尿液、脑脊髓液和其他生物学样本。其中使用最广泛的技 术是光学测量,实例包括比色、吸收、光谱测定和荧光检测方 法。可通过这些方式测量体液中的抗原…

  • RE: 白皮书下载丨ADI系列可穿戴解决方案助力生命体征监测!

    如果想了解更多ADI可穿戴解决方案,请下载↓

     PDF