How to configure the ADPD103 for Optical detection for measuring the Chemical flow and bubble detection
How to configure the ADPD103 for Optical detection for measuring the Chemical flow and bubble detection
Hi there,
For my project, I’m trying to optimize an optical sensor system which function is to recognize, wether there is a tube in the detection slit. The sensor is based on an emitting LED and a position sensitive device with 2 electrodes on the opposing…
Thanks Kevin. Together with ADPD105 Entry (as below), firmware update is quite easy.
Under CM3WSD, one should NOT forget the buttons (pressing Download button on the board while pulsing RESET button).
The schematic and provisions design, as well as the board itself, assignment writing companies indicate sign titles for easy classification. For further data on the functionality of the ADP103, lead to the ADP104 results covering.
Hi community,
I have set up a ADPD103 Evaluation Board with two photodiodes (PD1 and PD2) and one LED. I want to measure the intensity of the LED with both photodiodes. When i bring the LED close to PD1, the signal rises to high LSBs, but at the same…
按照ADPD103规格书的启动时序,在编程模式里使能了时钟(寄存器0x4B),LED和PD都配置为SLOTA,其他寄存器参数默认,然后去读寄存器0x64的值。
发现LED可以亮,但是0x64的值一直不变,把LED灭了,发现对0x64的值没有影响。
请问是不是还有什么特殊寄存器需要配置?