• RE: what's the meaning of "Vstart" in ADP7104 datasheet?

    Hello,

    VStart is the required input voltage at VIN which the ADP7104 requires to be operational. So to operate BOTH conditions have to be met:

    1. Vstart>=3.2V  (Part is operational)
    2. Vuvlo>=1,28V (Part is switched on)

    kind regards

    Markus

  • adp7104

    May I ask whether the device in the picture has a fixed output or an adjustable output

  • 关于ADP7104-3.3

        用ADP7104-3.3做了一个稳压器,输入5V,输出3.3V。正常工作时候电流约为70mA。输出端并了三个电容:一个3528 10V 100uF的钽电容(靠近输出引脚)、一个0603 1uF 陶瓷电容、一个0603 1nF的陶瓷电容。

       现在有一个问题:有钽电容的时候,电源电流异常,有600mA之多,拿掉钽电容,电源电流正常。

       实在搞不懂原因是什么,麻烦各位坛友分析一下,感谢!

  • ADP7104供电问题

    请问:看FMC那块用于SDR的板子原理图,其中用1个ADP7104给ADL5380和AD8366供电,5380工作时245mA,8366工作时180mA,用1个7104供电(500mA)会不会电流裕量留的太小?

  • adp7104输出电流问题

    ADI工程师:

    您好,ADP7104ARDZ-5.0 的数据手册上写了最大输出500ma电流,可是经过我的测试发现ADP7104ARDZ-5.0的输出电流最多只有160ma,我的负载是阻性负载, 很想知道为什么,请大家回答。

    下图是我的原理图

  • ADP7104电压输出不正常

    最近选用电源芯片ADP7104-5V。我的电路图如图所示:

    用万用表在芯片8脚可量得电压为8V

    但是量得芯片1脚的输出却为1.22V,不是我想希望得到的5V,请问这是什么原因?

    谢谢

  • ADP7104 and ADP151 input and output Capacitor

    Dear support,

    in my design I use ADP7104 and ADP151 linear regulator.

    In the figure 2 on pag.1 of the ADP7104 datasheet it reports an Electrolytic Capacitor, if I correctly understand,

    but on pag. 17 of the datasheet, it is written that ceramic…

  • Drive ADP7104 EN/UVLO with Digital I/O

    Can I drive the EN/UVLO pin with LVCMOS 3.3V logic from an FPGA? Before configuration, the FPGA I/O will either be high impedance or weak pull-down. Then after configuration, the I/O will be driven high to enable the regulator. Also, if I were to use…

  • 关于ADP7104电流输出能力问题


    ADP7104标称最大输出电流500MA,我按照DATASHEET上的参考电路进行设计,为什么输出只有100多mA?请各位大拿指导一下,ADI的工程师解决一下~

  • AD7902+ADP7104-2.5V组合工作电流过大

    按照芯片手册,AD7902的功耗最大只有12mW,而ADP7104的接地电流也很小,但是在使用工程中发现ADP7104与AD7902组合时,ADP7104的工作电流达到了75mA左右,有时甚至能超过100mA。电路我是参考了AD7902评估板的电路。具体如下:

    这部分我使用7.5V供电。