• ADP5585 going BAD after few days usage.ESD ISSUES?

    We are using ADP5585 in our design for interfacing to a keyboard. The schematics is as shown in the attachment. The lines KBC0,1,2,3 and KBR0,1,2,3 are going to a 4 X 4 matrix KEYPAD connected with about 15 inches long ribbon cable.

    The capacitors C2…

  • False Key Detection in ADP5585

    HI all.,

    We are facing a false key detection on our product. We are using the Keypad Decoder ADP5585 IC for the KEypad logic on our product.

    The datasheet of ADP5585 specifies that a Key press will be detected after a key scan during which the columns…

  • I have additional questions on the ADP5585.


    Hello,

    I would like to ask questions on the ADP5585 GPI.

    Q: Under the following condition, how can I figure out the times given below , respectively?

    Condition:  PSC_FREQ=00 => 50kHz,  Debounce filter enabled.

    1) time 1 :  The times from OSC_EN 

  • TWI/I2C repeat start read ADP5585 on BF537

    Dear Sir,

    I am trying to use ADP5585 as keypad decoder being used in our Project. I have successfully written data to it using I2C Interface. But I am having trouble reading data from it using repeated start. I don't know why I am not able to read data…

  • Hello , I would like to ask a question on ADP5585.

    Hello ,

    My questions about the ADP5585  are follows . Your advice would be appreciated.

    RST function

    1) Can the RST pin be released ( set HIGH) as soon as the power supply voltage has been reached its specified value?

    Or some wait time required ?

  • ADP5585 - no communication when interrupt onHey, I have a problem with ADP5585 - I can read status value, when I press button read event fifo then clear int flag etc, but when I want to use interrupt pin - I can't even read status register - always 0...

    Hey, I have a problem with ADP5585 - I can read status value, when I press button read event fifo then clear int flag etc, but when I want to use interrupt pin - I can't even read status register - always 0, device generate first interrupt and then I…

  • RE: ADP5587 SPEC. Question

    Hello Jacky,

    The ADP5587 has pull-ups enabled by default on start-up. The maximum recommended sink current is 1mA per pin.

    Other chips to consider are the ADP5585, ADP5586, and the ADP5589. These are able to source up to 5 mA and sink up to 10 mA per…

  • RE: ADP5587 Key Matrix

    Hello,

    1) For the keypad, we don't recommend using RC filters. The pins are well protected from ESD, and as long as the wires running to the KP pins are not ridiculously long, it should be good without filtering.

    2) The 100 kΩ resistors are not…

  • TAGS LIST: Interface and Isolation

    LTM2894
    LTM2895
    LTM9100
    LTM2885
    LTM2881
    LTM2882
    LTM2883
    LTM2884
    LTM2893
    LTM2886
    LTM2887
    LTM2889
    LTM2892
    LTC1694-1
    LTC4300
    LTC4310
    LTC4302
    LTC4305
    LTC4304
    LTC4303
    LTC4306
    LTC4307
    LTC4307-1
    LTC430…
  • 集坛友力量,破解零回复

    2017最后一个月的零回复问题如期而至,一起来集思广益,破解零回复~

    蛛丝马迹就在下方,哪里能逃过众多坛友的“火眼金睛”呢。

    走过路过,不要错过……

    现在就来浏览下方问题,你的回复将为你带来积分,被标记为“正确答案”或“有用答案”,会得到更高的积分哦~(ps.积分=礼物,请看 积分商城

    快快拿出你们的智慧、发动你身边的大神,为还在着急的坛友找到答案吧!

    放大器类产品

    如何提高AD8221交流耦合电路的信噪比、输入阻抗、共模抑制比

    滤波器设计 

    AD9524开发板USB连接不上电…