• [#5588] build adp5520 kernel fails

    [#5588] build adp5520 kernel fails

    Submitted By: Mingquan Pan

    Open Date

    2009-10-09 00:39:47     Close Date

    2010-01-03 23:39:28

    Priority:

    Medium     Assignee:

    Nobody

    Status:

    Closed     Fixed In Release:

    N/A

    Found In Release:

    2010R1     Release:

    Category:

    N/A     Board:

    N…

  • [#5228] adp5520 keys doesn't function on branch head kernel

    [#5228] adp5520 keys doesn't function on branch head kernel

    Submitted By: Mingquan Pan

    Open Date

    2009-06-11 00:23:55     Close Date

    2009-06-16 05:06:54

    Priority:

    Medium High     Assignee:

    Michael Hennerich

    Status:

    Closed     Fixed In Release:

    N/A

    Found In Release…

  • [#5015] kernel build fails when adp5520 is built into kernel but i2c is a module

    [#5015] kernel build fails when adp5520 is built into kernel but i2c is a module

    Submitted By: Mike Frysinger

    Open Date

    2009-03-25 22:59:55     Close Date

    2009-04-08 22:12:01

    Priority:

    Low     Assignee:

    Michael Hennerich

    Status:

    Closed     Fixed In Release:

    N/A

  • 2010-05-28 10:08:22     ADP5520 driver

    2010-05-28 10:08:22     ADP5520 driver

    Appalayagari Sreedhar (INDIA)

    Message: 89958   

    Hi,

    I am working with ADSP BF533 Custom board and 2009R1-RC1 distribution. In the custom board ADP5501 backlight chip is used for the LCD.

    I have enabled the adp5520…

  • 2010-09-03 03:50:33     ADP5520 chip support

    2010-09-03 03:50:33     ADP5520 chip support

    vijai ragavan (INDIA)

    Message: 93101   

    Hi,

    I am working on BF533 processor, I need to be validated the keypad which is connected to ADP5520 chip, I referred the document from the following link.

    https://docs…

  • ADP5520-EVALZ, software needed

    Hi,

    I was wondering if anyone can send me the ADP5520-EVALZ software? I can't find the installation CD in the box. Maybe I'd misplaced it.

    Regards,

    Xey

  • Using ADP5520 for driving SHARP LCD backlight

    Hi,

    We are planning to use the ADP5520 Backlight driving chip for our LCD panel - SHARP - LQ043T3DG01. Datasheet can be downloaded from here:

    http://www.google.co.in/url?sa=t&rct=j&q=sharp%20lq043t3dg01&source=web&cd=1&ved=0CDAQFjAA&url=http%3A%2F…

  • Reload bitstream in Zc706 on the fly from ARM

    We are developing  a custom design on Zc706 EVM using AD9680.

    I'd like to reload FPGA bitstreams on the fly from the ARM. But when I switch bitstreams the interface to the AD9680 no longer works.

    Inside /sys/bus/platform/drivers

    Xilinx Watchdog                axi…

  • FAQ: [#6864] Record in bf527-ezkit ssm2602 with S24_LE format, underrun will happen in 2011r1 branch(2011)

    [#6864] Record in bf527-ezkit ssm2602 with S24_LE format, underrun will happen in 2011r1 branch

    Submitted By: Vivi Li

    Open Date

    2011-10-31 06:33:55     Close Date

    2011-11-02 03:19:14

    Priority:

    Medium     Assignee:

    Scott Jiang

    Status:

    Closed     Fixed In Release:

  • FAQ: [#6739] Can't use S24_LE format to record audio with ssm2602 on bf527-ezkit-v2(2011)

    [#6739] Can't use S24_LE format to record audio with ssm2602 on bf527-ezkit-v2

    Submitted By: Vivi Li

    Open Date

    2011-08-23 04:55:26     Close Date

    2011-10-12 05:36:31

    Priority:

    Medium     Assignee:

    Scott Jiang

    Status:

    Closed     Fixed In Release:

    N/A

    Found In…