• adp5350

    Good afternoon,

    I want to know how much time take the change when i enter my data in the registers of the adp5350??

    thanks and best regards,

  • ADP5350

    Good afternoon,

    What i should i do when the charger status give me "Suspend" and THR status give "Battery Hot" ??

    For the THR status is always "Battery Hot" when EN_CHG is 'ON' or 'OFF'.

    Thanks,

  • ADP5350

    Good afternoon,

    I want to ask about the appropriate system load when the battery feed the system.

    Thanks and best regards,

  • adp5350 & LTspice

    Good morning,

    I want to ask adp5350 power management is available for LTspice. If it available how to add it to the LTspice component .

    Regards,

  • ADP5350 & LTspice

    Good morning ,

    I want to ask if there is a way to work with ADP5350 power management in LTspice because i search for the LTspice component i didn't found it .

    If there is way tell me how to do it.

    Best regards,  

  • ADP5350 FCC certification

    Hello,

    I need to know if the ADP5350 IC has a FCC certification.

    Regards,

  • Demo ADP5350 GUI

    Good Evening,

    I downloaded the labview and the Demo ADP5350 GUI. When i open the demo it give me a message "the vi is not executable. the complete labview development system is needed to correct errors".

     What will I do in this case?

    Thanks…

  • ADP5350

    Good afternoon,

    i want to ask how about the discharge of the battery. Is that the discharge work  only when disable the "EN_CHG" bit or plug out  the Vbus of the DC-DC charger.

    Thanks and regards,

  • adp5350

    Good morning,

    I use a a Li-ion Polymer Battery with model "HPL402323-2C-190mAh" (Vnominal = 3.7 V and C = 190 mA/h) for my system. i put my load in each output to simulate my system also i set the battery SOC (0%) with battery voltage 2.9 V and…

  • ADP5350

    Good afternoon,

    How can i did better accuracy in the battery SOC because when i set the the fual Gauge it give me a fault battery soc according to battery SOC curve ?

    for more detail see the following image 

    Best regards,