Hi Sagar,
Regarding the efficiency, you can refer to the user guide 4 and 5. it's better to connect SYS and BAT together.
You have to…
Hi Sagar,
Regarding the efficiency, you can refer to the user guide 4 and 5. it's better to connect SYS and BAT together.
You have to…
您好:Kevin.Yao@
1、我注意到datasheet第一页上“The ADP5091/ADP5092 provide efficient conversion of the harvested limited power from a 6 μW to 600 mW range with submicrowatt operation losses. ”5091可以从PV获得的最大功率就是600mW吗,或者更高?
2、请问如果我有一个太阳能电池,它的开路电压是5V,最大短路电流是150mA…
资源推荐
ADP5091/ADP5092 是一款智能集成式能量采集纳米电源管理解决方案,可转换来自PV电池或热电发生器(TEG)的直流电源。该器件可对储能元件(如可充电锂离子电池、薄膜电池、超级电容和传统电容)进行充电,并对小型电子设备和无电池系统上电。
ADP5091/ADP5092提供有限采集能量(从16 μW到600 mW范围)的高效转换,工作损耗为亚μW级别。 利用内部冷启动电路,调节器可在低至380 mV的输入电压下启动。 冷启动后,调节器便可在80 mV至3.3 V的输入电压范围内正常工作…
1) I'm not entirely sure how to understand REG_D0 and REG_D1 settings.
Table 6 "Regulated Output Working Mode Configuration" describes:
Working Mode | REG_D0 | REG_D1 |
Boost Disable | Low | Not applicable |
Boost Enable | High | Not applicab… |
LTM8045 |
LTM8049 |
LTM4651 |
LTM4661 |
LTM4686 |
LTM4676 |
LTM4686-1 |
LTM4676A |
LTM4675 |
LTM4677 |
LTM4678 |
LTM8062 |
LTM8061 |
LTM8052 |
LTM8026 |
LTM8056 |
LTM8064 |
LTM8054 |
LTM8055 |
LTM4600 |
LTM4600HV |
LTM4608A |
LTM4604A |
LTM8032 |
I am designing a very small 4 layer wireless device (34.25 mm x 20 mm) where the ADP509x is powering an STM MCU from a source like indoor solar. The small size means that space and weight are a big factor for component selection. Height of components is…
Hello, I just want to spread an hint. If you do not use the DIS_SW pin to disable the boost converter don´t leave it floating. Connect it to ground with a resistor or directly. Apparently there is no internal pulldown on this pin.