• Recommended footprint of ADP5072

    Hello


    Would you please share the data of the recommended footprint of ADP5072?
    I searched for symbols and footprints on the product page, but it didn't seem to be prepared.

    I would be grateful if you could reply.

    Bset Regards,
    Knj

  • Inductor Selection of ADP5072 Datasheet

    Hello

    There is a problem when I am solving DUTY, Ton, and Inductance Value(L1) for Inductor selection.

    I substituted the table 11 values in the ADP5072 Datasheet into the Inductor selection equation(in the ADP5072 Datasheet).

    Table 11 values are Vin…

  • RE: AD9129 VSSA (-1.5V) biasing

    Hello

    I like to generate -27V from ADP5072 with VIN of 12V. The datasheet states that Vout can be Vin-39V.

    Can you please confirm whether it is possible to generate -27V? If not, what negative voltage can be generated from +12V Vin supply? 

  • TAGS LIST: Power Management

    LTM8045
    LTM8049
    LTM4651
    LTM4661
    LTM4686
    LTM4676
    LTM4686-1
    LTM4676A
    LTM4675
    LTM4677
    LTM4678
    LTM8062
    LTM8061
    LTM8052
    LTM8026
    LTM8056
    LTM8064
    LTM8054
    LTM8055
    LTM4600
    LTM4600HV
    LTM4608A
    LTM4604A
    LTM8032
  • ADI 新品速递(2019 年 5 月)

    ADI 5月新产品上线,想了解的筒子们不要错过!

    0.5 dB LSB6 位硅数字衰减器,9 kHz 40 GHz

    ADRF5720 是一款 6 位数字硅衰减器,以 0.5 dB 步长提供 31.5 dB 的衰减控制范围。该器件的工作频率范围为 9 kHz 至 40 GHz,提供优于 4.5 dB 的插入损耗和出色的衰减精度。在所有状态下,ADRF5720 的 ATTIN 端口具有 27 dBm(平均值)和 30 dBm(峰值)的射频 (RF) 输入功率处理能力。

    主要特性

    • 超宽带频率范围…
  • 超全产品合集丨ADI 2019年度硬核新品大集结,码起来慢慢看!

    马上就是农历新年,在2019年里你都做了些啥呀~而ADI为了满足各位工程师不断变化的设计需求,从没停下新品发布的脚步。今天斑竹为大家盘点下2019年来ADI发布的硬核新品,看看咱们ADI工程师这一年来杠杠的成果吧~

    小尺寸、高效率、低噪声、单片同步 4A 降压型 DC/DC 转换器 LTC3308A 

    LTC3308A 采用 2.25V 至 5.5V 输入电源,在高达 3 MHz 的开关频率下使用恒定频率峰值电流模式控制,最短接通时间低至 22 ns,可通过小型外部元件实现快速瞬态响应。Silent Sw…